This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请教DSP6678 两个网口同时使用NDK的问题



                      请教DSP6678 两个网口同时使用NDK的问题

      在新板卡中,6678连接了两个网口到交换,但是在使用NDk协议时,找不到如何同时设置这两个网口的地方。

      在NDK相关函数中,不知哪个函数可以用来指定网口0和1,如何同时配置?谢谢!

       rc = NC_SystemOpen( NC_PRIORITY_LOW, NC_OPMODE_INTERRUPT );

       hCfg = CfgNew();

       CfgAddEntry( hCfg, CFGTAG_SYSINFO, CFGITEM_DHCP_HOSTNAME, 0,
                 strlen(HostName), (UINT8 *)HostName, 0 );

          bzero( &NA, sizeof(NA) );
        //NA.IPAddr  = inet_addr(LocalIPAddr);
        NA.IPAddr  = inet_addr(IPAddr_by_Mac);
        NA.IPMask  = inet_addr(LocalIPMask);
        strcpy( NA.Domain, DomainName );
        NA.NetType = 0;

        // Add the address to interface 1
        CfgAddEntry( hCfg, CFGTAG_IPNET, 1, 0,
                           sizeof(CI_IPNET), (UINT8 *)&NA, 0 );

        // Add the default gateway. Since it is the default, the
        // destination address and mask are both zero (we go ahead
        // and show the assignment for clarity).
        bzero( &RT, sizeof(RT) );
        RT.IPDestAddr = 0;
        RT.IPDestMask = 0;
        RT.IPGateAddr = inet_addr(GatewayIP);

        // Add the route
        CfgAddEntry( hCfg, CFGTAG_ROUTE, 0, 0,
                           sizeof(CI_ROUTE), (UINT8 *)&RT, 0 );

       NC_NetStart( hCfg, NetworkOpen, NetworkClose, NetworkIPAddr );