大家好,
我们基于DM385 IPNC3.5的软件版本,在SPI0,CS0上接了一块flash,后来发现,DM385的SPI接口的MISO,MOSI和flash的DI,DO接反了,导致flash读写失败,请问通过软件能交换MISO和MOSI管脚吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
大家好,
我们基于DM385 IPNC3.5的软件版本,在SPI0,CS0上接了一块flash,后来发现,DM385的SPI接口的MISO,MOSI和flash的DI,DO接反了,导致flash读写失败,请问通过软件能交换MISO和MOSI管脚吗?
您好,
1.信号线上有33欧电阻,起隔离作用。
2.flash上的D0/D1飞线互换后,flash通了,可读写,用示波器看了波形也正常。
3.在论坛搜spi会出现很多这样的问题,不过是其他arm平台的,例如am335x,但是解决办法都相同。