This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM8148 选型问题



2 Channel video input,one raw data,one 640*480p50.

1. SD卡的读取速度是多少

2. 是否支持触摸屏,分辨率多少

3. OSD,Video信号是否可以叠加一起处理

4. 芯片工作范围,现在看到是商业级范围

5. 是否有GUI提供

6. 能否支持Android系统

  • 该问题线下已经回复。建议使用ISS话,使用DM8127参考设计。

    1.       SD卡的读取速度是多少

    [Chris] Pls check processors.wiki.ti.com/.../TI81XX_PSP_04.04.00.01_Feature_Performance_Guide.

    2.       是否支持触摸屏,分辨率多少

    [Chris] No SW support now. Need customer to implement.

    3.       OSD,Video信号是否可以叠加一起处理

    [Chris] Yes.

    4.       芯片工作范围,现在看到是商业级范围

    [Chris] Yes. There is industry level chip for DM8127.

    5.       是否有GUI提供

    [Chris] No in IPNC reference design.

    6.       能否支持Android系统

    [Chris] No in IPNC reference design.