This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM8127 主码流1920X1440分辨率死机问题



我们采用DM8127自制版,内存为1G。ISS模块接收1920X1440YUV422数据,经过resize后得到两路数据:

第一路数据放大到2048X1536,然后进行缩小得到一路D1数据和一路512X384数据,其中512X384这路数据和前面的2048X1536数据一起送给DSP进行处理,得到的数据结果送给m3Video进行JPEG编码,同时前面这路D1数据添加OSD后,dup后一份送给m3video进行H.264编码,得到子码流,另一份进行显示输出。

第二路数据可以放大到2048X1536,也可以缩小为1920X1080,或者直接输出1920X1440,添加OSD后,进行H.264编码,得到主码流。

目前出现一个问题,就是当主码流分辨率为1920X1440时,系统运行16天9小时33分左右出现死机,串口,网络均没有响应,显示输出也没有图像;而在此时间之前,系统一切运行正常。但是当主码流分辨率为2048X1536时,系统一切运行正常。

请教TI的工程师一下,这个问题可能出现的原因是什么?