This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM2732: AM2732不启动

Part Number: AM2732
Other Parts Discussed in Thread: AWR2243, TIDA-020047

AM2732上电概率不启动定位,请帮忙给一些排查建议。

1、         平台说明

参考TIDA-020047,am2732+awr2243级联板;

FLASH型号:GD25Q64EWIGR

Sop配置:SOP[4:0]=00001

2、         问题现象

出现上电后AM2732概率不启动,可以量到时钟有40mhz,调试串口无数据输出。

3、         定位过程

  1. 异常时抓取复位信号ok;
  2. 异常时抓取SOP4:0均正常

  1. 上电时序OK 、电源也掉干净了。

  1. 测量QSPI_cs信号无拉低。

图表 1 正常启动时的CS信号

图表 2 异常时的CS信号无拉低

  • 我迅速对照了GD25Q64EWIGR NOR闪存的规格书,该存储器似乎没有专用的硬件复位引脚,同时在AM273x TRM/设备初始化/启动过程/启动模式章节中也发现了以下说明

    所以我有一些问题:
    Q1.由于AM273x ROM不支持GD25Q64EWIGR软件重置启用(0x66)和重置(0x99)命令,在设备在热重置或软件启动的冷重置后重新启动的情况下,如何在TIDA-020047上将重置信息传递给GD25Q64 EWIGR?ROM启动时,存储器寄存器应处于干净状态。
    Q2.在电路板上电并首次成功启动后,多次断言热复位信号输入warm_reset的行为是什么?SBL重新启动是否成功?
    Q3.您是否也有NRESET输入(是黄色RST信号?)、3V3_FLASH电源、40 MHz系统参考时钟(OSCCLKOUT)和WARM_RESET输出的波形图,这些输出是在通电后启动失败时显示的?

  • 没有收到后续回复。