This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

J784S4XEVM: J784S4XEVM Booting Linux via EMMC UDA fail

Part Number: J784S4XEVM

HI!

https://software-dl.ti.com/jacinto7/esd/processor-sdk-rtos-j784s4/11_01_01_01/exports/docs/pdk_j784s4_11_01_00_17/docs/userguide/j784s4/boot/boot_app.html

    Refer to the above chapter Booting Linux via MMCSD booting the system normally, but Booting Linux via EMMC UDA failed!

    The kernel can boot normally but the file system failed to enter. The file system is in sd.

    All mirrors use sdk and have not been modified.

    error Log:

    mmc0: running CQE recovery

    Unable to handle kernel NULL pointer dereference at virtual address 0000000000000000