This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAPL138运行NDK例程helloWorld出现问题



您好!

       我是NDK使用的新手,最近在测试NDK的例子helloworld时,出现如下情况:

      

TCP/IP Stack 'Hello World!' Application

Using MAC Address: 00-01-02-03-04-05
EMAC should be up and running 
EMAC has been started successfully
Registeration of the EMAC Successful
Service Status: DHCPC : Enabled : : 000
Service Status: DHCPC : Enabled : Running : 000
Link Status: 100Mb/s Full Duplex on PHY 1
Service Status: DHCPC : Enabled : Fault : 002

我使用的是CCSv5.4,ndk版本是ndk_2_22_03_20,nsp版本是nsp_1_10_02_09,BIOS版本是bios_6_35_01_29,用的是第三方的评估板,运行的例程是ndk_evm6748_coff_helloWorld工程

看NDK user's guide手册上说这个程序成功运行后会打印IP地址,但我这并没有打印IP地址

我查找了很多解决方法,但是几个月过去还是没进展,希望得到您的帮助,谢谢您!