我是按照bb black 烧写全纪录 操作的,现在烧写一部分之后出现这种情况,请问这是什么情况
[ 1.987426] Detected MACID=a0:f6:fd:8b:a4:d7
[ 1.992828] cpsw: Detected MACID = a0:f6:fd:8b:a4:d9
[ 1.998931] omap_rtc am33xx-rtc: setting system clock to 2000-01-01 00:00:01 UTC (946684801)
[ 2.019226] Freeing init memory: 9572K
[ 2.023498] Failed to execute /init
[ 2.027496] Kernel panic - not syncing: No init found. Try passing init= option to kernel. See Linux Documentation/init.txt for guidance.
[ 2.040527] Backtrace:
[ 2.043121] [<c0017dbc>] (dump_backtrace+0x0/0x10c) from [<c041b628>] (dump_stack+0x18/0x1c)
[ 2.051971] r6:c004203c r5:c04febf8 r4:c0f68048 r3:c0f1df0c
[ 2.057922] [<c041b610>] (dump_stack+0x0/0x1c) from [<c041b864>] (panic+0x64/0x194)
[ 2.065948] [<c041b800>] (panic+0x0/0x194) from [<c041b5ec>] (init_post+0xac/0xd0)
[ 2.073883] r3:df02bc00 r2:00000009 r1:00000080 r0:c04febf8
[ 2.079833] r7:00000013
[ 2.082519] [<c041b540>] (init_post+0x0/0xd0) from [<c05a1900>] (kernel_init+0xf8/0x120)
[ 2.090972] r4:c05dc388 r3:c0f65340
[ 2.094787] [<c05a1808>] (kernel_init+0x0/0x120) from [<c004203c>] (do_exit+0x0/0x65c)