This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于C6678共享L2 SRAM的问题请教



大家好:

        我对于C6678的L2 SRAM(0x00800000)以及各个core私有的L2 SRAM(core 0::0x10800000,core1:0x11800000),存在些疑问,想请教下大家,测试代码框图如下:

        int a=0;

        if(selfId==0)

       {

      a=a+1;

         }

      else if((1<=selfId)&&(selfId<=6))

     {

     a=a+2;

     }

   else

   {

   a=a+3;

   }

   以上是一个很简单的测试代码,selfId是由CSL_chipReadReg()函数获取的核号,我想通过观察a改变后的值来了解共有L2 SRAM和私有L2 SRAM的关系,通过.map文件得知a变量的地址是0x00844b30。

   测试结果如下:

     L2 SRAM(0x00844b30)的值随着core 0的L2 SRAM(0x10844b30)的值改变而改变,每次增加1(以上代码会一直执行) ,它们俩的值相同;而core 1~core6(0x11844b30~0x16844b30)的值每次增加2,core7(0x17844b30)的值每次增加3;

  问题如下:

    为什么全局变量a在L2 SRAM(0x00844b30)的值随着core 0对它的改变而改变,而不随着其他几个核改变?L2 SRAM(0x00800000)仅仅对于core 0的L2 SRAM(0x10800000)是一种映射关系吗?而对于其他7个core的L2 SRAM不存在映射关系?

   

   谢谢!

  • 对于core 0,0x00844b30是local address,0x10844b30是Global address,这两地址物理上是一样的;

    但是core 1想访问core 0的0x00844b30的L2 地址就必须使用0x10844b30,如果core 1使用0x00844b30实际访问的是0x11844b30,以此类推。