This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

dm368 uboot emac



你好!我使用的是 dvsdk_dm368_4_02_00_06中的u-boot  

PHY 使用是DM9161

启动后打印

DM36x initialization passed!

TI UBL Version: 1.50

Booting Catalog Boot Loader

BootMode = NAND

Starting NAND Copy...

Valid magicnum, 0xA1ACED66, found in block 0x00000019.

  DONE

Jumping to entry point at 0x81080000.

U-Boot 2010.12-rc2 (Jul 12 2012 - 01:00:54)

Cores: ARM 432 MHz

DDR:   340 MHz

I2C:   ready

DRAM:  128 MiB

NAND:  256 MiB

MMC:   davinci: 0, davinci: 1

Bad block table found at page 65472, version 0x01

Bad block table found at page 131008, version 0x01

Bad block table found at page 65408, version 0x01

Bad block table found at page 130944, version 0x01

nand_read_bbt: Bad block at 0x000003120000

nand_read_bbt: Bad block at 0x00000b120000

NAND read from offset 3c0000 failed -74

*** Warning - readenv() failed, using default environment

Net:   Read from EEPROM @ 0x50 failed

DaVinci-EMAC

Hit any key to stop autoboot:  0

就停止了  

没有打印任何PHY 的东西。是不是需要配置EMAC ?