This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

dm8127 YCbCr 16bit 输入?



dm8127 的Camera Interface (I/F)支持YCbCr 16bit的吗?

9.12 Imaging Subsystem (ISS)

Parallel Camera (CAM) interface features:
– Input format
• Bayer pattern Raw (up to 16bit) or YCbCr 422 (8bit or 16bit) data.

在硬件上哪8bit是Y,哪8bit是 CbCr?

Video Input (Digital)也是支持YCbCr 16bit的输入,这两个接口有什么区别?

sensor可以输出parallel YCbCr 16bit,是不是这两个接口都可以用?

  • alex_xu 说:
    dm8127 的Camera Interface (I/F)支持YCbCr 16bit的吗?

    可以

    alex_xu 说:
    在硬件上哪8bit是Y,哪8bit是 CbCr?

    请参考ISS文档的ISS ISP VP Format Mapping。Data【15:0】-》Y【7:0】,C【7:0】

    alex_xu 说:

    Video Input (Digital)也是支持YCbCr 16bit的输入,这两个接口有什么区别?

    sensor可以输出parallel YCbCr 16bit,是不是这两个接口都可以用?

    是的。但是ISS的IPIPE还可以对YUV镜像EE等处理。