EVM6678板块上,我设置的是sw6、sw5、sw4、sw3(0000 0000 0000 1101),但是连接上仿真器之后,查看0x02620020=0x80b。我SW6~sw3设置为全0时,0x02620020=0x0。而且我用万用表测量拨
码开关的电平,没有问题,为啥连上仿真器之后,通过这0x02620020地址查看到的就成了0x80b呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
EVM6678板块上,我设置的是sw6、sw5、sw4、sw3(0000 0000 0000 1101),但是连接上仿真器之后,查看0x02620020=0x80b。我SW6~sw3设置为全0时,0x02620020=0x0。而且我用万用表测量拨
码开关的电平,没有问题,为啥连上仿真器之后,通过这0x02620020地址查看到的就成了0x80b呢?
要错开一位,DEVSTAT的bit1才对应BOOTMODE的bit0, DEVSTAT的bit 0是大小端模式选择位
@zhengdongli
我知道sw6~sw3的对应关系,但是我设置的sw6~sw3为0000 0000 0000 1011(i2c的0x50地址启动)根据http://processors.wiki.ti.com/index.php/TMDXEVM6678L_EVM_Hardware_Setup这里的文档即
4. Pin 4 of SW5 is the I2C address pin (off: 0x51, on: 0x50) for I2C boot mode,可是通过DEVSTAT读出来就是0x80b,那么ccs就识别到就是boot方式就是i2c基于0x51启动,而不是我通过sw6~sw3设置的i2c 的0x50地址启动,因此我在evm6678l板块上总上无法实现i2c的0x50自举。
请问你是否遇到过这样的问题。