This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于Compiler7.4的安装问题



我原来搞2000系列产品,一个多月前开始转C6678,想搞HPC。本想5月初能设计并制作板子,现在看来要推迟到本月底了。

我不但已经看完所有相关技术手册,还在技术支持社区的帮助下得到了诸如vkfft、KI底层软件和IPC应用程序等,但有一件事至今还在困扰着我:

我一个月前拿到C6678EVM板子后,就按照过去搞2000系列的习惯,所有的活动全部局限在附带光盘内。发现很多重要的示例程序都需要Compiler7.4,而且后来在技术支持社区获得的程序也大都需要Compiler7.4,但光盘安装的环境中只有Compiler7.3.4,所以这些示例程序根本无法Import到CCS中。害得我只能用notepad看程序,上次还不小心把头文件注释中的省略号看成是程序的一部分。

开始我不想通过CCS更新,因电脑是XP不想被病毒感染,所以就单独下载了Compiler7.4,但安装时屏幕一闪,什么也未发生。后来向销售商要了新的序列号,在win7电脑里通过CCS更新Compiler,怎么搞都不行,白白浪费整整一晚上。最后只好拿自己的XP工作电脑上网通过CCS更新,没想到花费近一个上午,还是不行。现在我用的还是Compiler7.3.4,很多示例程序还是没法使用。现在的计划是先看懂程序,然后重新建立工程,看能否通过。

无论如何,我还是想安装Compiler7.4的,连8.2版的都装好了,难道7.4版就不能安装,请各位协助,有了7.4我们的进展就会加快。