This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请问为什么显示没有源文件,而且下载程序也下载不进去呢?No source available for "0xff8000"



为什么显示没有源文件,而且下载程序也下载不进去呢? 使用的5509a

No source available for "0xff8000" 

MEMORY
{
PAGE 0:
PROG0(RWX) : origin = 04000h length = 08000h
P_VECT(RIX) : origin = 0FF80h length = 00100h
PAGE 1:
DATA0(RW) : origin = 0C000h length = 04000h
}

SECTIONS
{
.vectors : { } > P_VECT PAGE 0
.text : { } > PROG0 PAGE 0
.cinit : { } > PROG0 PAGE 0
.csldata : { } > DATA0 PAGE 1
.stack : { } > DATA0 PAGE 1
.sysstack : { } > DATA0 PAGE 1
.bss : { } > DATA0 PAGE 1
.cio : { } > DATA0 PAGE 1
.const : { } > DATA0 PAGE 1
.sysmem : { } > DATA0 PAGE 1
}