This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ccs3.3&dm642

编译软件 CCS3.3 芯片DM642 ,connect 过程中 先Reseting 然后就直接disconnect 出现以下错误,请问这是可能哪地方出现问题?
Trouble Writing Memory Block at 0x1800020 on Page 0 of Length 0x4: Error 0x00000022/-1154 Error during: Memory, Execution, The memory at 0x00000000 continually indicated it was 'not ready' The emulator was unable to regain control of the processor. The processor must be reset. Sequence ID: 66 Error Code: -1154 Error Class: 0x00000022

在GEL文件中 将GEL_MapAdd( 0x01800000, 0, 0x00000058, 1, 1 ); // EMIFA CTL REGS 注释掉后 ,编译软件处于HALTED 。提示如下错误:

GEL: Error while executing OnTargetConnect(): memory map prevented write to target memory at 0x01800000.

打开工程后 编译下载后 提示如下错误,但是不影响简单程序的运行:
GEL: Error while executing OnTargetConnect(): memory map prevented write to target memory at 0x01800000.
GEL: Error calling OnPreFileLoaded(): memory map prevented write to target memory at 0x01800000

  • 请问用的是EVM板还是自己的板子?什么仿真器?

    为什么 要把EMIFA CTL REGS注释掉?

  • 使用的是自己做的板子、 仿真器 用的是 XDS510。 注释那句 因为报错总是提示0X1800000 那有问题,仿真器和板子 连接不上。 注释掉后 就可以连接了。 请问下 会是什么问题呢?

  • 可能是芯片工作不稳定,测量一下芯片的电源,复位信号,晶振,CLKOUT4/CLKOUT6是否有正确的时钟输出? JTAG信号是否都正常。