请教TI的工程师。用的是OMAPL138片子,编译器用的ccs V6.0;DSP生成.out文件后,如何配置.bat文件来直接用.out文件生成bin文件。我看到网上有人这么做的,写好cmd文件,然后再配置好.bat批处理程序,用DOS直接生成bin文件。希望得到指教
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
可以写成bat批处理文件,在DOS下运行AISgen_d800k008.exe,见下面bootloader user guide里的说明。
5.3.11 Command Line Usage
The AISgen tool supports command line usage to facilitate the automation. To run AISgen from a terminal
window, follow this procedure:
1. Create a configuration file (*.cfg) using the GUI. This file will specify all parameters needed to generate
an AIS file, including the input and output file names.
2. Open a terminal window and navigate to the AISgen directory.
3. Run AISgen with the following usage:
AISgen_d800k008.exe –cfg=”<CFG file
name>”
This procedure allows quick generation of an updated AIS image after modifying the underlying application
or binary input files.