This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MCSDK用户指导手册中提供下载开发包的网址无法打开



MCSDK用户指导手册中提供下载开发包的网址无法打开 jdl.com/.../dtc-v1.3.0.tgz  想下载dtc-v1.3.0.tgz 压缩包

  • 建议在linux环境下下载,附件是我在linux下下载后传到window的一个压缩包供参考。

    dtc-v1.3.0.7z
  • 根据网站提示,make以后出现下列错误并没有生成The 'dtc' and 'ftdump' executables ,怎么解决?

    root@ubuntu:/opt/ti/dtc-v1.3.0# make all
    LEX convert-dtsv0-lexer.lex.c
    make: flex: Command not found
    BISON dtc-parser.tab.c
    make: bison: Command not found
    LEX dtc-lexer.lex.c
    make: flex: Command not found
    CHK version_gen.h

  • 你有执行下一步将-WALL去掉么,我给你的压缩包已经编译过了,你不编译直接用看可以不。

    1. Edit dtc-v1.3.0/Makefile to remove -Wall from the WARNINGS macro
  • Hi,你好

    谢谢您提供的压缩包,可以帮我在解决一个问题吗?

    编译目录:
    <mcsdk_install_path>/pdk_keystone2_3_01_03_06/packages/ipc-transport/linux/qmss

    编译生成ARMv7 Linux TransportQmss Tests工程出现错误,参考下面链接网址ARMv7 Linux TransportQmss Source Delivery and Recompilation部分,进行编译

    http://processors.wiki.ti.com/index.php/MCSDK_UG_Chapter_Developing_Transports#Recompiling_Through_GIT_Repository_2

    1. 通过GIT方式获取源码,Recompiling Through GIT Repository,首先安装了mcsdk_linux_3_01_04_07/linux-devkit-rt目录下的arago-*****-sdk-i686.sh脚本,安装目录/opt/ti/arago
    2. git clone得到的文件,安装在了***/pdk_keystone2_3_01_04_07/packages目录下,按照网站提示修改了armv7setupenv.sh文件linaro toolchain 和 installed devkit path ,如图1-1所示

    图1-1

    3. 其中交叉编译器已在/etc/bash.bashrc中设置完成

    4. 按照操作步骤更新文件source armv7setupenv.sh,并进入目录/ipc-transport/linus/qmss后,执行完$make lib 和$ make tests,会出现如图1-2所示错误,无法链接动态库

    图1-2

    NOTE:Setting the USEDYNAMIC_LIB environment variable to "yes" will generate the shared library test executables 
    $ export USEDYNAMIC_LIB=yes
    已经在/ipc-transport/linus/qmms下的makefile和/test/build/makefile
    以及/build/armv7/libTransportQmss_aearmv7.mk中都加入了export USEDYNAMIC_LIB=yes,依然有错误

  • Hi,您好

    在PDK_keystone的开发包中,有没有简单的DSP和ARM的通信例程,需要DSP和ARM相互读写数据