This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

win10系统下TMDSEVM6670LE6670LE评估版无法连接PC



实验室买了几块TMDSEVM6670LE评估板,送来的板子应该是TMDSEVM6670L的板子,片上仿真器为xds100,通过JTAG仿真接头外接了XDS560v2的仿真器板子(如图所示)

在安装驱动之后(XDS560V2)  设备管理器无法识别,如图所示

test按钮 显示:

[Start]

Execute the command:

%ccs_base%/common/uscif/dbgjtag.exe -f %boarddatafile% -rv -o -F inform,logfile=yes -S pathlength -S integrity

[Result]


-----[Print the board config pathname(s)]------------------------------------

C:\Users\sfm\AppData\Local\.TI\1387006483\
0\0\BrdDat\testBoard.dat

-----[Print the reset-command software log-file]-----------------------------

This utility has selected a 560/2xx-class product.
This utility will load the program 'bh560v2u.out'.
E_RPCENV_IO_ERROR(-6) No connection: emulator was not found
Download failed for file G:\TI\ccsv5\ccs_base\common\uscif\xds560v2.out

An error occurred while soft opening the controller.

-----[An error has occurred and this utility has aborted]--------------------

This error is generated by TI's USCIF driver or utilities.

The value is '-250' (0xffffff06).
The title is 'SC_ERR_ECOM_EMUNAME'.

The explanation is:
An attempt to access the named emulator via USCIF ECOM has failed.

[End]

CCS5.4版本 安装完好

请问是win10系统不兼容导致的吗?还是别的原因?有解决方法吗? 

望回复 

谢谢!