RT!
哪家公司有推出SPI FLASH的开发板,FLASH最好是用M25P128的片子,多片FLASH最好,现在手上有个这样的项目,都是老片子了,请知道的大神们提供些信息,或者提供一些移植资料。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
RT!
哪家公司有推出SPI FLASH的开发板,FLASH最好是用M25P128的片子,多片FLASH最好,现在手上有个这样的项目,都是老片子了,请知道的大神们提供些信息,或者提供一些移植资料。
谢谢你,还有一个问题请教一下:
一直被一个问题困扰着,就是ARM核要用SPI的EDMA,DSP核要用mcasp的EDMA,但是这两个EDMA通道怒属于同一个edma控制器,但是手册上写着同一个edma控制器有4个EDMA3_0_CC0_INT[3:0],但是在库.h的中断向量表里面同一个EDMA控制器只有一个中断完成向量,两个核可以同时用中断的方式使用同一个EDMA通道控制器的不同通道吗?比如ARM用SPI EDMA中断方式,DSP用MCASP EDMA中断方式,如果可以的话怎么用?因为我在库文件里面只找到一个中断向量,但是芯片手册里面有4个中断向量。
谢谢你,还有一个问题请教一下:
一直被一个问题困扰着,就是ARM核要用SPI的EDMA,DSP核要用mcasp的EDMA,但是这两个EDMA通道怒属于同一个edma控制器,但是手册上写着同一个edma控制器有4个EDMA3_0_CC0_INT[3:0],但是在库.h的中断向量表里面同一个EDMA控制器只有一个中断完成向量,两个核可以同时用中断的方式使用同一个EDMA通道控制器的不同通道吗?比如ARM用SPI EDMA中断方式,DSP用MCASP EDMA中断方式,如果可以的话怎么用?因为我在库文件里面只找到一个中断向量,但是芯片手册里面有4个中断向量。