This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SRIO启动失败

Other Parts Discussed in Thread: SYSBIOS

C6678,自制板子,外挂DDR3,使用SYS/BIOS,运行在DDR3中,使用仿真器在线仿真SRIO能够正常启动,和FPGA通信也正常,整个程序正常运行。

做离线,spi flash中存放两段程序,二级boot 以及应用程序,二级boot通过RBL启动成功,然后二级boot初始化DDR,加载应用程序,跳转到应用程序运行,现在问题是,应用程序运行到Srio_start时产生异常,去掉SRIO初始化部分,程序能够正常启动运行。

异常如下:

[C66xx_0] Memory Region 0 Initialized
Memory Region 1 Initialized
QMSS successfully initialized
CPPI successfully initialized
PA successfully initialized
A0=0x800009e0 A1=0x0
A2=0x0 A3=0x80002a80
A4=0x1 A5=0x2e10
A6=0x1 A7=0x12
A8=0x1 A9=0xc102338
A10=0x800009e0 A11=0x80434ce0
A12=0x0 A13=0x0
A14=0x80407e38 A15=0xb3e4021d
A16=0x85f870 A17=0x0
A18=0x85f68c A19=0x1e0
A20=0x0 A21=0x0
A22=0x0 A23=0x0
A24=0x0 A25=0x0
A26=0x0 A27=0x0
A28=0x1085fc50 A29=0x134
A30=0x34022e10 A31=0x1085fc50
B0=0x0 B1=0x4
B2=0x0 B3=0x80415466
B4=0x81 B5=0x2a02a00
B6=0x80 B7=0x188
B8=0x0 B9=0xc10232c
B10=0x80002bc0 B11=0xffffffff
B12=0x6f B13=0xda
B14=0x80488310 B15=0x85f928
B16=0x0 B17=0x0
B18=0x2e00000 B19=0x0
B20=0x0 B21=0x2e0
B22=0x2e00000 B23=0x0
B24=0x0 B25=0x3000
B26=0x3000 B27=0x0
B28=0x0 B29=0x0
B30=0x2e0 B31=0x4
NTSR=0x1800f
ITSR=0xd
IRP=0x80415162
SSR=0x0
AMR=0x0
RILC=0x0
ILC=0x0
Exception at 0x80414cc0
EFR=0x40000000 NRP=0x80414cc0
ti.sysbios.family.c64p.Exception: line 255: E_exceptionMin: pc = 0x80414cc0, sp = 0x0085f928.
To see more exception detail, use ROV or set 'ti.sysbios.family.c64p.Exception.enablePrint = true;'
xdc.runtime.Error.raise: terminating execution