CCS V6.1
EVM6657L
mcsdk_2_01_02_06
串口工具:HyperTerminal和SecureCrt
1.按照read me文档将mcsdk中POST例程通过I2C下到EEPROM,bus address 0x50,重新上电前,将Boot Mode Dip Switch Settings拨到I2C POST boot模式,
| I2C POST boot | (off, off, on, off, on, on, on, on) |
(on, on, on, on, on, on, on, on) |
上电后串口工具无显示;重复多次均无显示;
2.然后再将mcsdk中POST例程通过I2C下到EEPROM,bus address 0x51,重新上电前,将Boot Mode Dip Switch Settings拨到I2C boot模式( 0x51)
| I2C boot | (off, off, on, off, on, on, on, on) |
(on, on, on, off, on, on, on, on) |
上电后串口成功显示POST自检信息;
3.在此条件下,重新执行1中的0x50模式,上电后串口亦成功显示POST自检信息;
4.将IBL通过I2C下到EEPROM,bus address 0x51后,再执行1中的0x50模式,上电后串口工具再次无显示;
5.IBL NOR boot on image 0 (default)和IBL NAND boot on image 0上电后,串口工显示正常。
还请各位大神不吝赐教,谢谢!