This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

如何实现时间分片轮转的调度算法?



<1>芯片:C6655

<2>开发板:自己设计的开发板,参考TI的设计

<3>要实现的目的:在单核上实现取流和解码,相机帧率为10,I帧间隔为12,要求1秒内解码出5帧图像;

<4>尝试的方案:

(1)每秒钟前几百毫秒取够5帧图像后解码,这样的话算法分析的图像又不是实时的,因为算法每次只分析一帧;

(2)模拟时间分片的调度算法,取流和解码这两个任务的切换时间从1微秒到100ms都尝试过,都发现了取流丢包的情况?

<5>问题:TI工程师和各位朋友,有在单核CPU上实现过时间分片轮转调度算法,并运用于取流和解码的吗,如果说这个方案可行的话,需要注意哪些地方才能做到不丢包?