自己设计的板子,使用的DDR3型号为4片MT41J128M16HA125。芯片频率是1600M,现配置PHY的参数如下:
现在对这个DQS和CK的值有些疑问,不知道这个值是否指的就啊PCB上的6678到芯片相应拐角的长度?还有就是不知道这个DQS_ECC和CK_ECC应该怎么看呢?下面是我通过表格计算出来的ddr3初始化的值。
ps:写个简单的测试程序,发现写不进去数,我知道这肯定是我配置有问题,但就是不知道该怎么进行查找,还请专家帮忙解答下,谢谢了
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
DDR3初始化参考SPRABL2 KeyStone DDR3 Initialization手册,或者参考首页STK里DDR3初始化流程;
另外1600有问题可以先试试1333或者1066;
ECC没有的话可以不管,因为你的DDR3配置里ECC开关肯定是关闭的,控制器不会采用该参数计算。
请问一下,如果我的板子只外接了一篇DDR3 K4B1G1646E ,那么excel表格里的 Ck1到 CK0,还有 DQS2到DQS7, DQSECC,CKECC 的值是不是全部写0