TMS320C6410: Need archived C6000 CGT v6.2.21 Windows compiler for legacy CCS3 TMS320C6410 project

Part Number: TMS320C6410

I have a legacy CCS3.3 library project targeting TMS320C6410 DSP.

 

The project uses legacy compiler flags -pdsw225 and -mv6400+, which are only supported by C6000 CGT v6.2.x series.

 

Newer CGT v7/v8/v20 compilers do not recognize these old flags and will break the original code optimization behavior.

 

The official download page has archived v6.x compiler versions and no public download link is available now.

 

Could you please send the archived download link of ti_cgt_c6000_6.2.21_windows_installer.exe to my account?