This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6678电源设计问题汇总,请专家帮忙解答,谢谢!

Other Parts Discussed in Thread: UCD9244, UCD7242, UCD74111, UCD9222

各位专家好:

最近正在调试基于6678的板子,C6678电源设计问题汇总,请专家帮忙解答,谢谢!

1.硬件设计时没有留PMbus接口,只是6678的VID接口与UCD9244相连,上次技术工程师来我们单位,说可以通过DSP的电源控制模块,通过程序和VID接口就可以实现电源管理,但是我在Mcsdk中没有找到关于UCD电源配置的例程,请问编程时需要编写电源方面的程序吗?要编写的程序的功能是烧写UCD9244内部的Flash还是实时控制电源电压,还是SmartReflex自动管理(不用编程),硬件接上就行了?

2.UCD9244内部的Flash必须配置吗?第一次上电时肯定没配置,那岂不是要出错,DSP起不来就不能配置,不配置DSP就起不来,这不是先有蛋还是先有鸡的问题吗?配置一次就可以了还是每次都要配置啊?UCD9244内部的Flash为空估计DSP也能起来吧?

3.对电源控制芯片UCD9244的必须的配置包括什么?手册里看到可以配置VID_lockout_interval ,手册里还说VID的接口模式,4bit,6bit,8bit是由PMbus command决定的,我感觉应该是对电压电流配置,但是既然是浮动电压的,为什么还要配置那?

4.

关于供电设计,硬件设计手册中提到使用UCD7242,但是从散热设计及热功耗性能考虑,推荐大家在设计时改用UCD74111。如果是视频应用,UCD7242供电能力余量不足,必须使用UCD74111,这是真的吗?我照开发板的设计不行吗?

最近把论坛帖子读遍了,没找到答案,麻烦了。

谢谢!