This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM335x 双网口,一个正常另一个不停的up,down

Other Parts Discussed in Thread: AM3354

am3354 接了2个网口(phy都为lan8710a),采用同一个时钟(am3354输出25MHz),现在的情况是:网口0能正常工作,网口1不停的在up/down:

phyCORE-AM335x login: [ 10.427795] PHY: 0:01 - Link is Up - 100/Full
[ 14.427764] PHY: 0:01 - Link is Down
[ 16.427795] PHY: 0:01 - Link is Up - 100/Full
[ 20.427764] PHY: 0:01 - Link is Down
[ 23.427764] PHY: 0:01 - Link is Up - 100/Full
[ 27.427764] PHY: 0:01 - Link is Down
[ 30.427764] PHY: 0:01 - Link is Up - 100/Full
[ 34.427734] PHY: 0:01 - Link is Down
[ 36.427764] PHY: 0:01 - Link is Up - 100/Full
[ 40.427764] PHY: 0:01 - Link is Down

可能会是什么问题呢?

谢谢!