This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EVMK2H开发板的网口1不通



各位专家好,

        我在使用EVMK2H开发板时遇到了如下问题:

        将开发板设置为no-boot,在C66X核上运行MCSDK中的helloworld工程,直接可以ping通 mac port0;

        但是连接到mac port 1时,就没法ping通了。了解到helloworld使用了platform、ndk等库,修改了platform的内容,将emac_init中的phy的部分改为初始化sgmii(1),并修改ndk中的nimu库,设置TxPort为1,重新生成了platform库和ndk库,依然没法ping通。

        请问EVMK2H上面两个以太网口的区别是什么,在使用时有哪些要注意的地方,与ARM核运行还是DSP核运行有关系吗,如果想启用板子的port 1,应该怎么做,要修改哪些地方?

        谢谢!