This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ti-processor-sdk-linux-am335x-evm-02.00.02.11编译错误



Linux系统信息:

Linux ubuntu 4.2.0-27-generic #32~14.04.1-Ubuntu SMP Fri Jan 22 15:32:26 UTC 2016 x86_64 x86_64 x86_64 GNU/Linux

make时出错,信息如下:

=====================================
Building the Linux Kernel DTBs
=====================================
make -C /home/yong/ti-processor-sdk-linux-am335x-evm-02.00.02.11/board-support/linux-4.1.18+gitAUTOINC+bbe8cfc1da-gbbe8cfc ARCH=arm CROSS_COMPILE=/home/yong/ti-processor-sdk-linux-am335x-evm-02.00.02.11/linux-devkit/sysroots/x86_64-arago-linux/usr/bin/arm-linux-gnueabihf- tisdk_am335x-evm_defconfig
make[1]: Entering directory `/home/yong/ti-processor-sdk-linux-am335x-evm-02.00.02.11/board-support/linux-4.1.18+gitAUTOINC+bbe8cfc1da-gbbe8cfc'
HOSTCC scripts/basic/fixdep
In file included from /home/yong/ti-processor-sdk-linux-am335x-evm-02.00.02.11/linux-devkit/sysroots/cortexa8hf-vfp-neon-linux-gnueabi/usr/include/features.h:402:0,
from /home/yong/ti-processor-sdk-linux-am335x-evm-02.00.02.11/linux-devkit/sysroots/cortexa8hf-vfp-neon-linux-gnueabi/usr/include/sys/types.h:25,
from scripts/basic/fixdep.c:106:
/home/yong/ti-processor-sdk-linux-am335x-evm-02.00.02.11/linux-devkit/sysroots/cortexa8hf-vfp-neon-linux-gnueabi/usr/include/gnu/stubs.h:7:29: fatal error: gnu/stubs-soft.h: No such file or directory
# include <gnu/stubs-soft.h>
^
compilation terminated.
make[2]: *** [scripts/basic/fixdep] Error 1
make[1]: *** [scripts_basic] Error 2
make[1]: Leaving directory `/home/yong/ti-processor-sdk-linux-am335x-evm-02.00.02.11/board-support/linux-4.1.18+gitAUTOINC+bbe8cfc1da-gbbe8cfc'
make: *** [linux-dtbs] Error 2

谢谢!