This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6748 upp发送问题?



您好:

  目前正在使用C6748的UPP功能,可是出现了一个很奇怪的问题;如下图所示:

在约循环2ms的中断程序中发送如上图for循环中的数据就会使程序崩溃,注意里面第一个字是65535;

再看下图,for循环里面第一个字改成0,程序运行就会一切正常,为什么会这样呢?它就仅仅是一个数据而已,不知道跟CacheWB函数有没有关系,

另外,再之前已经将DDR、L1/L2配置成了CACHE,求解答,谢谢!