This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

am335x QML移植



使用几个ti的sdk都无法使用qml。有没有相关的教程移植QT5 QML到335x,没有使用TI SDK的文件系统,是自己做的debian系统。

如果QT_QPA_DEFAULT_PLATFORM = linuxfb,可以显示qt程序,但qml需要opengl,则需要QT_QPA_DEFAULT_PLATFORM = eglfs,执行程序出现错误,无法初始化显示egl

  • 关键问题是qt5了,你只能看看最新的sdk了,我记得里面是有移植了。

  • 最新的是有 移植,我想请问,你们ti的rootfs是如何制作的,以及里面的qt移植过程,有没有相关教程,你们的rootfs太大了

  • 关于QT的移植,目前能找到的资源:

    http://processors.wiki.ti.com/index.php/Qt_4_to_5_Migration

    http://processors.wiki.ti.com/index.php/Building_Qt?keyMatch=qt5&tisearch=Search-EN

    我们rootfs的制作是基于Yocto的,制作过程比较长,可以参考这个:

    http://arago-project.org/wiki/index.php/Setting_Up_Build_Environment

    如果可以使用我们默认提供的,建议你还是用默认提供的比较快捷。我们有两个rootfs,一个是tisdk的,比较大;还有一个是arago base的,比较小的。小的印象中大概是几十M的样子,这个还是太大的话,就需要考虑剪裁了。

  • 你好,我发现你们ti-processor-sdk-linux-am335x-evm-01.00.00.03里的rootfs关于SGX Graphics SDK这部分内容与按照http://processors.wiki.ti.com/index.php/Graphics_SDK_Quick_installation_and_user_guide然后生成的是不一样的,是不是你们的rootfs做过这部分修改,而且后面每个ti-processor-sdk-linux-am335x的rootfs关于Graphics_SDK的内容都不太一样。我按照http://processors.wiki.ti.com/index.php/Graphics_SDK_Quick_installation_and_user_guide这个教程,第一次启动,然后执行./335x-demo,

    Installation complete!

    You may now reboot your target.

    [ 53.222658] PVR: PVRCore_Init

    [ 53.226391] PVR: PVRSRVDriverProbe(pDevice=dd8cca00)

    [ 53.233640] PVR: SGX register base: 0x56000000

    [ 53.238141] PVR: SGX register size: 16777215

    [ 53.242498] PVR: SGX IRQ: 53

    [ 53.246236] PVR: EnableSystemClocks: Enabling System Clocks

    [ 53.252861] PVR: GPTIMER11 clock is 24MHz

    [ 53.259246] PVR: PVRCore_Init: major device 248

    [ 53.310316] PVR: Installing MISR with cookie bf05e670

    [ 53.315626] PVR: Installing device LISR SGX ISR on IRQ 53 with cookie ddc83180

    [ 53.324093] PVR: SysFinalise: Version string: SGX revision = 125

    PVR:

    PVR: Memory Stats

    PVR: ------------

    PVR:

    PVR: High Water Mark = 0 bytes

    Loaded PowerVR consumer services.

    PVR SGX是加载成功了,而且运行OGLES2ChameleonMan这个程序也是可以的。但是关机重启后,就出现

    PVR: PVRCore_Init
    [    5.322573] PVR: PVRSRVDriverProbe(pDevice=dd8cca00)
    [    5.327809] PVR: SGX register base: 0x56000000
    [    5.332372] PVR: SGX register size: 16777215
    [    5.336675] PVR: SGX IRQ: 53
    [    5.399930] PVR: EnableSystemClocks: Enabling System Clocks
    [    5.405596] PVR: GPTIMER11 clock is 24MHz
    [    5.409674] Unhandled fault: external abort on non-linefetch (0x1028) at 0xfa04a054
    [    5.417367] Internal error: : 1028 [#1] ARM
    [    5.421567] Modules linked in: pvrsrvkm(O+)
    [    5.425785] CPU: 0 PID: 1409 Comm: systemd-udevd Tainted: G           O 3.14.43-g875c69b #1
    [    5.434172] task: ddc18000 ti: ddc8e000 task.ti: ddc8e000
    [    5.439935] PC is at AcquireGPTimer+0x158/0x250 [pvrsrvkm]
    [    5.445560] LR is at OSMapPhysToLin+0xb8/0xec [pvrsrvkm]
    [    5.450893] pc : [<bf0483a4>]    lr : [<bf02acc8>]    psr: a00d0013
    [    5.450893] sp : ddc8fbf8  ip : ddc8fbc8  fp : ddc8fc34
    [    5.462417] r10: c0074f58  r9 : ddc8e000  r8 : 0000000e
    [    5.467659] r7 : bf05b82c  r6 : 00000000  r5 : bf05b82c  r4 : dd8cca10
    [    5.474211] r3 : fa04a054  r2 : dc9ce458  r1 : 00000000  r0 : fa04a054
    [    5.480764] Flags: NzCv  IRQs on  FIQs on  Mode SVC_32  ISA ARM  Segment user
    [    5.487926] Control: 10c5387d  Table: 9dbc8019  DAC: 00000015
    [    5.493693] Process systemd-udevd (pid: 1409, stack limit = 0xddc8e238)
    [    5.500332] Stack: (0xddc8fbf8 to 0xddc90000)
    [    5.504705] fbe0:                                                       600d0013 bf05d60c
    [    5.512917] fc00: 600d0013 bf05e79c dc9ce458 4804a054 dd80bd00 fa04a054 00000000 016e3600
    [    5.521129] fc20: dd80bd00 bf020550 ddc8fc54 ddc8fc38 bf0485a8 bf048258 bf031ebc bf05e670
    [    5.529341] fc40: ddce8840 bf05e79c ddc8fc9c ddc8fc58 bf048f04 bf048538 ddc8fc7c ddc8fc68
    [    5.537553] fc60: c00246a0 c00221f0 dd8cdf00 bf05e670 00000000 bf05e670 ddba8000 ddce88d4
    [    5.545764] fc80: bf05e80c 00000000 00000000 0000000b ddc8fcc4 ddc8fca0 bf027404 bf048928
    [    5.553976] fca0: ddc8fcbc dd8cca00 00000000 00000000 c07d50b4 dd8cca10 ddc8fcdc ddc8fcc8
    [    5.562188] fcc0: c0356d8c bf027330 c0838d70 dd8cca10 ddc8fd04 ddc8fce0 c03558b4 c0356d78
    [    5.570399] fce0: 00000000 dd8cca10 bf05b82c dd8cca44 00000000 bf077000 ddc8fd24 ddc8fd08
    [    5.578611] fd00: c0355a6c c03557b0 dd8c593c 00000000 bf05b82c c03559d8 ddc8fd4c ddc8fd28
    [    5.586823] fd20: c0353ff8 c03559e4 dd863d8c dd8c5930 ddedcfb4 bf05b82c ddedcf80 c07f0028
    [    5.595035] fd40: ddc8fd5c ddc8fd50 c03553ac c0353fa8 ddc8fd84 ddc8fd60 c0354fb4 c0355394
    [    5.603246] fd60: bf053454 ddc8fd70 bf05b82c bf05b97c 00000000 ddebe200 ddc8fd9c ddc8fd88
    [    5.611458] fd80: c03560f0 c0354ee4 ddc8ff48 bf05b97c ddc8fdac ddc8fda0 c0356ce0 c035607c
    [    5.619670] fda0: ddc8fdf4 ddc8fdb0 bf0770b0 c0356c9c c0096d84 c00950d0 ddc8fddc ddc8fdc8
    [    5.627882] fdc0: c05785c8 c0577384 c008ed30 ffffffff ddc8fdec ddc8fde0 c008ed28 c0578470
    [    5.636093] fde0: ddc8fe1c ddc8fdf0 ddc8fe84 ddc8fdf8 c0008858 bf07700c 00000000 00000000
    [    5.644305] fe00: bf05b970 00000000 bf05b970 c0074f58 ddc8fe44 ddc8fe20 c057b328 c057bc20
    [    5.652516] fe20: ffffffff c07d87f0 ddc8fe44 ddc8fe38 c005aaf8 c005b728 ddc8fe6c ddc8fe48
    [    5.660728] fe40: c0051710 c005aaf4 00000000 ddc8fe58 ddc8ff48 bf05b97c 00000001 ddc8ff48
    [    5.668939] fe60: bf05b97c 00000001 ddebe200 00000001 bf05b970 c0074f58 ddc8ff44 ddc8fe88
    [    5.677151] fe80: c00776d0 c0008770 bf05b97c 00007fff c0075180 00000000 ddc8fec4 e0b01000
    [    5.685363] fea0: 00000000 bf05b97c 00000000 e0d91934 ddc8fedc ddc8e000 bf05b9b8 bf05ba9c
    [    5.693575] fec0: c0074d94 c0756d14 e0b01000 0035553f 00012755 00000000 0b300002 bf049d34
    [    5.701786] fee0: 00000002 00000000 00000000 00000000 00000000 00000000 00000000 00000000
    [    5.709997] ff00: 00000000 00000000 00000000 00000000 00000000 00000000 00001ab8 00000000
    [    5.718209] ff20: 00000007 b6da69f8 0000017b c000e904 ddc8e000 00000000 ddc8ffa4 ddc8ff48
    [    5.726420] ff40: c0077f08 c0076074 e0b01000 0035553f e0d91254 e0d910bf e0e504e4 0005e888
    [    5.734633] ff60: 0006d188 00000000 00000000 00000000 0000002c 0000002d 00000017 00000014
    [    5.742844] ff80: 0000000e 00000000 c00085f0 00000000 be8e2014 00000000 00000000 ddc8ffa8
    [    5.751055] ffa0: c000e780 c0077ea8 00000000 be8e2014 00000007 b6da69f8 00000000 00000000
    [    5.759267] ffc0: 00000000 be8e2014 00000000 0000017b 00020000 00037f78 00050048 0006a088
    [    5.767479] ffe0: be8e1ef0 be8e1ee0 b6da0c4b b6eabb42 800e0030 00000007 00000000 00000000
    [    5.775684] Backtrace:
    [    5.778396] [<bf04824c>] (AcquireGPTimer [pvrsrvkm]) from [<bf0485a8>] (EnableSystemClocks+0x7c/0x8c [pvrsrvkm])
    [    5.788845] [<bf04852c>] (EnableSystemClocks [pvrsrvkm]) from [<bf048f04>] (SysInitialise+0x5e8/0x7bc [pvrsrvkm])
    [    5.799349] [<bf04891c>] (SysInitialise [pvrsrvkm]) from [<bf027404>] (PVRSRVDriverProbe+0xe0/0x108 [pvrsrvkm])
    [    5.809577] [<bf027324>] (PVRSRVDriverProbe [pvrsrvkm]) from [<c0356d8c>] (platform_drv_probe+0x20/0x50)
    [    5.819110] [<c0356d6c>] (platform_drv_probe) from [<c03558b4>] (driver_probe_device+0x110/0x234)
    [    5.828015]  r5:dd8cca10 r4:c0838d70
    [    5.831618] [<c03557a4>] (driver_probe_device) from [<c0355a6c>] (__driver_attach+0x94/0x98)
    [    5.840086]  r8:bf077000 r7:00000000 r6:dd8cca44 r5:bf05b82c r4:dd8cca10 r3:00000000
    [    5.847893] [<c03559d8>] (__driver_attach) from [<c0353ff8>] (bus_for_each_dev+0x5c/0x90)
    [    5.856100]  r6:c03559d8 r5:bf05b82c r4:00000000 r3:dd8c593c
    [    5.861804] [<c0353f9c>] (bus_for_each_dev) from [<c03553ac>] (driver_attach+0x24/0x28)
    [    5.869836]  r6:c07f0028 r5:ddedcf80 r4:bf05b82c
    [    5.874489] [<c0355388>] (driver_attach) from [<c0354fb4>] (bus_add_driver+0xdc/0x1d8)
    [    5.882442] [<c0354ed8>] (bus_add_driver) from [<c03560f0>] (driver_register+0x80/0xfc)
    [    5.890474]  r7:ddebe200 r6:00000000 r5:bf05b97c r4:bf05b82c
    [    5.896179] [<c0356070>] (driver_register) from [<c0356ce0>] (__platform_driver_register+0x50/0x64)
    [    5.905258]  r5:bf05b97c r4:ddc8ff48
    [    5.908937] [<c0356c90>] (__platform_driver_register) from [<bf0770b0>] (PVRCore_Init+0xb0/0x344 [pvrsrvkm])
    [    5.918879] [<bf077000>] (PVRCore_Init [pvrsrvkm]) from [<c0008858>] (do_one_initcall+0xf4/0x150)
    [    5.927803] [<c0008764>] (do_one_initcall) from [<c00776d0>] (load_module+0x1668/0x1d40)
    [    5.935923]  r10:c0074f58 r9:bf05b970 r8:00000001 r7:ddebe200 r6:00000001 r5:bf05b97c
    [    5.943808]  r4:ddc8ff48
    [    5.946359] [<c0076068>] (load_module) from [<c0077f08>] (SyS_finit_module+0x6c/0x78)
    [    5.954218]  r10:00000000 r9:ddc8e000 r8:c000e904 r7:0000017b r6:b6da69f8 r5:00000007
    [    5.962103]  r4:00000000
    [    5.964656] [<c0077e9c>] (SyS_finit_module) from [<c000e780>] (ret_fast_syscall+0x0/0x30)
    [    5.972863]  r6:00000000 r5:be8e2014 r4:00000000
    [    5.977515] Code: e34b3f05 ebff60d0 ea000030 e51b3020 (e5933000)
    [    5.983636] ---[ end trace b35156b3e34a1b4a ]---
    请问这是什么原因导致的

  • 你的QT 搞好了啊?我现在运行就发现:

    QML debugging is enabled. Only use this in a safe environment.
    This application failed to start because it could not find or load the Qt platform plugin "xcb"
    in "".

    Available platform plugins are: eglfs, linuxfb, minimal, minimalegl, offscreen.

    Reinstalling the application may fix this problem.
    Aborted

    我放了platforms 文件夹在同一目录也是这样的。。。。

  • 你好! 请问以下这个问题,最后是怎么解决的! 我现在也出现了一样问题!

    root@am335x-evm:/etc/init.d# ./335x-demo
    0x10205
    debug8.x
    /dev/mem opened.
    Memory mapped at address 0xb6fc4000.
    Read at address  0x44E0007C (0xb6fc407c): 0x00030000
    Write at address 0x44E0007C (0xb6fc407c): 0x00000002, readback 0x00000002
    installing 8.x SGX debug user libraries

    Installing PowerVR Consumer/Embedded DDK 'sgxddk_1.10@2359475' on target

    File system installation root is /

    Uninstalling existing version sgxddk_1.10@2359475
    Uninstallation completed.
    boot script rc.pvr -> /etc/init.d/rc.pvr
    kernel module pvrsrvkm.ko -> /lib/modules/3.14.26-g07d13c6-dirty/extra/pvrsrvkm.ko
    kernel module omaplfb.ko -> /lib/modules/3.14.26-g07d13c6-dirty/extra/omaplfb.ko
    shared library libGLES_CM.so -> /usr/lib/libGLES_CM.so.1.10.2359475
    shared library libusc.so -> /usr/lib/libusc.so.1.10.2359475
    shared library libGLESv2.so -> /usr/lib/libGLESv2.so.1.10.2359475
    shared library libglslcompiler.so -> /usr/lib/libglslcompiler.so.1.10.2359475
    shared library libIMGegl.so -> /usr/lib/libIMGegl.so.1.10.2359475
    shared library libEGL.so -> /usr/lib/libEGL.so.1.10.2359475
    shared library libpvr2d.so -> /usr/lib/libpvr2d.so.1.10.2359475
    shared library libpvrPVR2D_BLITWSEGL.so -> /usr/lib/libpvrPVR2D_BLITWSEGL.so.1.10.2359475
    shared library libpvrPVR2D_FLIPWSEGL.so -> /usr/lib/libpvrPVR2D_FLIPWSEGL.so.1.10.2359475
    shared library libpvrPVR2D_FRONTWSEGL.so -> /usr/lib/libpvrPVR2D_FRONTWSEGL.so.1.10.2359475
    shared library libpvrPVR2D_LINUXFBWSEGL.so -> /usr/lib/libpvrPVR2D_LINUXFBWSEGL.so.1.10.2359475
    shared library libpvrEWS_WSEGL.so -> /usr/lib/libpvrEWS_WSEGL.so.1.10.2359475
    shared library libpvrEWS_REMWSEGL.so -> /usr/lib/libpvrEWS_REMWSEGL.so.1.10.2359475
    shared library libsrv_um.so -> /usr/lib/libsrv_um.so.1.10.2359475
    shared library libsrv_init.so -> /usr/lib/libsrv_init.so.1.10.2359475
    shared library libPVRScopeServices.so -> /usr/lib/libPVRScopeServices.so.1.10.2359475
    shared library libews.so -> /usr/lib/libews.so.1.10.2359475
    binary pvrsrvctl -> /usr/local/bin/pvrsrvctl
    binary sgx_init_test -> /usr/local/bin/sgx_init_test
    binary ews_server -> /usr/local/bin/ews_server
    binary ews_server_es2 -> /usr/local/bin/ews_server_es2
    binary services_test -> /usr/local/bin/services_test
    binary sgx_blit_test -> /usr/local/bin/sgx_blit_test
    binary sgx_clipblit_test -> /usr/local/bin/sgx_clipblit_test
    binary sgx_flip_test -> /usr/local/bin/sgx_flip_test
    binary sgx_render_flip_test -> /usr/local/bin/sgx_render_flip_test
    binary pvr2d_test -> /usr/local/bin/pvr2d_test
    binary gles1test1 -> /usr/local/bin/gles1test1
    binary gles1_texture_stream -> /usr/local/bin/gles1_texture_stream
    binary gles2test1 -> /usr/local/bin/gles2test1
    shader glsltest1_vertshader.txt -> /usr/local/bin/glsltest1_vertshader.txt
    shader glsltest1_fragshaderA.txt -> /usr/local/bin/glsltest1_fragshaderA.txt
    shader glsltest1_fragshaderB.txt -> /usr/local/bin/glsltest1_fragshaderB.txt
    binary gles2_texture_stream -> /usr/local/bin/gles2_texture_stream
    binary eglinfo -> /usr/local/bin/eglinfo
    binary ews_test_gles1 -> /usr/local/bin/ews_test_gles1
    binary ews_test_gles2 -> /usr/local/bin/ews_test_gles2
    shader ews_test_gles2_main.vert -> /usr/local/bin/ews_test_gles2_main.vert
    shader ews_test_gles2_main.frag -> /usr/local/bin/ews_test_gles2_main.frag
    shader ews_test_gles2_pp.vert -> /usr/local/bin/ews_test_gles2_pp.vert
    shader ews_test_gles2_pp.frag -> /usr/local/bin/ews_test_gles2_pp.frag
    binary ews_test_swrender -> /usr/local/bin/ews_test_swrender

    Installation complete!
    You may now reboot your target.

    Module pvrsrvkm failed to load. Retrying.
    Running /sbin/depmod
    [  107.771134] PVR: PVRCore_Init
    [  107.781950] PVR: PVRSRVDriverProbe(pDevice=df0cda00)
    [  107.787394] PVR: SGX register base: 0x56000000
    [  107.792146] PVR: SGX register size: 16777215
    [  107.796646] PVR: SGX IRQ: 53
    [  107.801183] PVR: EnableSystemClocks: Enabling System Clocks
    [  107.807564] PVR: GPTIMER11 clock is 24MHz
    [  107.815887] PVR: PVRCore_Init: major device 245
    [  107.963840] PVR: Installing MISR with cookie bf0cf120
    [  107.969576] PVR: Installing device LISR SGX ISR on IRQ 53 with cookie dc2b6ec0
    [  107.977672] PVR: SysFinalise: Version string: SGX revision = 125
    PVR:
    PVR: Memory Stats
    PVR: ------------
    PVR:
    PVR: High Water Mark = 0 bytes
    Loaded PowerVR consumer services.

    重启之后出现同样问题:

    [    8.217225] Bluetooth: L2CAP socket layer initialized
    [    8.304138] Bluetooth: SCO socket layer initialized
    [    8.555001] (stc):  chnl_id list empty :4
    [    8.559133] (stk) : st_kim_start(stk) :ldisc_install = 1
    [    9.149530] PVR: PVRCore_Init
    [    9.203519] PVR: PVRSRVDriverProbe(pDevice=df0cda00)
    [    9.208967] PVR: SGX register base: 0x56000000
    [    9.213707] PVR: SGX register size: 16777215
    [    9.218197] PVR: SGX IRQ: 53
    [    9.561840] PVR: EnableSystemClocks: Enabling System Clocks
    [    9.689962] (stk) :ldisc installation timeout
    [    9.694384] (stk) :ldisc_install = 0[    9.776374] PVR: GPTIMER11 clock is 24MHz
    [    9.935011] Unhandled fault: external abort on non-linefetch (0x1028) at 0xfa04a054
    [    9.943083] Internal error: : 1028 [#1] ARM
    [    9.947478] Modules linked in: pvrsrvkm(O+) btwilink ti_am335x_adc bluetooth kfifo_buf industrialio 6lowpan_iphc
    [    9.958216] CPU: 0 PID: 915 Comm: udevd Tainted: G           O 3.14.26-g07d13c6-dirty #66
    [    9.966811] task: df4ee000 ti: df538000 task.ti: df538000
    [    9.972857] PC is at AcquireGPTimer+0x158/0x250 [pvrsrvkm]
    [    9.978703] LR is at OSMapPhysToLin+0xb8/0xec [pvrsrvkm]
    [    9.984283] pc : [<bf0b8a30>]    lr : [<bf09ad4c>]    psr: a00f0013
    [    9.984283] sp : df539bf8  ip : df539bc8  fp : df539c34
    [    9.996341] r10: c0078088  r9 : df538000  r8 : 00000013
    [   10.001828] r7 : bf0cc2e0  r6 : 00000000  r5 : bf0cc2e0  r4 : df0cda10
    [   10.008685] r3 : fa04a054  r2 : dc028458  r1 : 00000000  r0 : fa04a054
    [   10.015543] Flags: NzCv  IRQs on  FIQs on  Mode SVC_32  ISA ARM  Segment user
    [   10.023038] Control: 10c5387d  Table: 9f53c019  DAC: 00000015
    [   10.029075] Process udevd (pid: 915, stack limit = 0xdf538238)
    [   10.035202] Stack: (0xdf539bf8 to 0xdf53a000)
    [   10.039776] 9be0:                                                       600f0013 bf0ce0bc
    [   10.048368] 9c00: 600f0013 bf0cf24c dc028458 4804a054 df00bd00 fa04a054 00000000 016e3600
    [   10.056963] 9c20: df00bd00 bf090550 df539c54 df539c38 bf0b8c34 bf0b88e4 bf0a2500 bf0cf120
    [   10.065559] 9c40: dc2041c0 bf0cf24c df539c9c df539c58 bf0b9590 bf0b8bc4 df539c7c df539c68
    [   10.074152] 9c60: c00254bc c0022f08 df0ceec0 bf0cf120 00000000 bf0cf120 dc46cc00 dc204254
    [   10.082744] 9c80: bf0cf2bc 00000000 00000000 0000000b df539cc4 df539ca0 bf097404 bf0b8fb4
    [   10.091339] 9ca0: df539cbc df0cda00 00000000 00000000 c0898248 df0cda10 df539cdc df539cc8
    [   10.099935] 9cc0: c033a62c bf097330 c0902560 df0cda10 df539d04 df539ce0 c0339154 c033a618
    [   10.108531] 9ce0: 00000000 df0cda10 bf0cc2e0 df0cda44 00000000 bf0e8000 df539d24 df539d08
    [   10.117124] 9d00: c033930c c0339050 df0c6a3c 00000000 bf0cc2e0 c0339278 df539d4c df539d28
    [   10.125715] 9d20: c0337894 c0339284 df064d8c df0c6a30 dc41b9b4 bf0cc2e0 dc41b980 c08b0c60
    [   10.134312] 9d40: df539d5c df539d50 c0338c4c c0337844 df539d84 df539d60 c0338854 c0338c34
    [   10.142906] 9d60: bf0c3c9c df539d70 bf0cc2e0 bf0cc430 00000000 df592c40 df539d9c df539d88
    [   10.151501] 9d80: c0339990 c0338784 df539f48 bf0cc430 df539dac df539da0 c033a580 c033991c
    [   10.160098] 9da0: df539df4 df539db0 bf0e80b0 c033a53c dfddad80 c08d1320 df539ddc df539dc8
    [   10.168691] 9dc0: c05d92e8 c05d80a4 c0091e28 ffffffff df539dec df539de0 c0091e20 c05d9190
    [   10.177287] 9de0: df539e1c df539df0 df539e84 df539df8 c00088b8 bf0e800c 00000000 00000000
    [   10.185882] 9e00: bf0cc424 00000000 bf0cc424 c0078088 df539e44 df539e20 c05dc028 c05dc920
    [   10.194479] 9e20: ffffffff c089b7f0 df539e44 df539e38 c005dbbc c005e7ec df539e6c df539e48
    [   10.203075] 9e40: c0054780 c005dbb8 00000000 df539e58 df539f48 bf0cc430 00000001 df539f48
    [   10.211670] 9e60: bf0cc430 00000001 df592c40 00000001 bf0cc424 c0078088 df539f44 df539e88
    [   10.220264] 9e80: c007a800 c00087d0 bf0cc430 00007fff c00782b0 00000000 df539ec4 e0f2e000
    [   10.228859] 9ea0: 00000000 bf0cc430 00000000 e11c23cc df539edc df538000 bf0cc46c bf0cc550
    [   10.237453] 9ec0: c0077ec4 c07bc5d4 e0f2e000 0035a3f7 0012c6e5 00000000 0000000e bf0ba3c0
    [   10.246047] 9ee0: 00000002 00000000 00000000 00000000 00000000 00000000 00000000 00000000
    [   10.254643] 9f00: 00000000 00000000 00000000 00000000 00000000 00000000 00001ae0 00000000
    [   10.263238] 9f20: 00000005 b6f8eb84 0000017b c000e964 df538000 00000000 df539fa4 df539f48
    [   10.271835] 9f40: c007b038 c00791a4 e0f2e000 0035a3f7 e11c1cec e11c1b5a e128231c 0005f338
    [   10.280431] 9f60: 0006dcc8 00000000 00000000 00000000 0000002c 0000002d 00000017 00000014
    [   10.289021] 9f80: 0000000e 00000000 00000000 00000000 00000000 00000000 00000000 df539fa8
    [   10.297616] 9fa0: c000e7e0 c007afd8 00000000 00000000 00000005 b6f8eb84 00000000 b6f8f93c
    [   10.306211] 9fc0: 00000000 00000000 00000000 0000017b b6f8eb84 00000000 0004b9b8 0004bc08
    [   10.314805] 9fe0: bec8da50 bec8da40 b6f86bc4 b6f078f0 800f0010 00000005 00000000 00000000
    [   10.323393] Backtrace:
    [   10.326264] [<bf0b88d8>] (AcquireGPTimer [pvrsrvkm]) from [<bf0b8c34>] (EnableSystemClocks+0x7c/0x8c [pvrsrvkm])
    [   10.337146] [<bf0b8bb8>] (EnableSystemClocks [pvrsrvkm]) from [<bf0b9590>] (SysInitialise+0x5e8/0x7bc [pvrsrvkm])
    [   10.348084] [<bf0b8fa8>] (SysInitialise [pvrsrvkm]) from [<bf097404>] (PVRSRVDriverProbe+0xe0/0x108 [pvrsrvkm])
    [   10.358719] [<bf097324>] (PVRSRVDriverProbe [pvrsrvkm]) from [<c033a62c>] (platform_drv_probe+0x20/0x50)
    [   10.368601] [<c033a60c>] (platform_drv_probe) from [<c0339154>] (driver_probe_device+0x110/0x234)
    [   10.377840]  r5:df0cda10 r4:c0902560
    [   10.381574] [<c0339044>] (driver_probe_device) from [<c033930c>] (__driver_attach+0x94/0x98)
    [   10.390360]  r8:bf0e8000 r7:00000000 r6:df0cda44 r5:bf0cc2e0 r4:df0cda10 r3:00000000
    [   10.398452] [<c0339278>] (__driver_attach) from [<c0337894>] (bus_for_each_dev+0x5c/0x90)
    [   10.406966]  r6:c0339278 r5:bf0cc2e0 r4:00000000 r3:df0c6a3c
    [   10.412880] [<c0337838>] (bus_for_each_dev) from [<c0338c4c>] (driver_attach+0x24/0x28)
    [   10.421213]  r6:c08b0c60 r5:dc41b980 r4:bf0cc2e0
    [   10.426036] [<c0338c28>] (driver_attach) from [<c0338854>] (bus_add_driver+0xdc/0x1d8)
    [   10.434287] [<c0338778>] (bus_add_driver) from [<c0339990>] (driver_register+0x80/0xfc)
    [   10.442621]  r7:df592c40 r6:00000000 r5:bf0cc430 r4:bf0cc2e0
    [   10.448535] [<c0339910>] (driver_register) from [<c033a580>] (__platform_driver_register+0x50/0x64)
    [   10.457954]  r5:bf0cc430 r4:df539f48
    [   10.461779] [<c033a530>] (__platform_driver_register) from [<bf0e80b0>] (PVRCore_Init+0xb0/0x344 [pvrsrvkm])
    [   10.472199] [<bf0e8000>] (PVRCore_Init [pvrsrvkm]) from [<c00088b8>] (do_one_initcall+0xf4/0x150)
    [   10.481454] [<c00087c4>] (do_one_initcall) from [<c007a800>] (load_module+0x1668/0x1d40)
    [   10.489878]  r10:c0078088 r9:bf0cc424 r8:00000001 r7:df592c40 r6:00000001 r5:bf0cc430
    [   10.498052]  r4:df539f48
    [   10.500697] [<c0079198>] (load_module) from [<c007b038>] (SyS_finit_module+0x6c/0x78)
    [   10.508849]  r10:00000000 r9:df538000 r8:c000e964 r7:0000017b r6:b6f8eb84 r5:00000005
    [   10.517022]  r4:00000000
    [   10.519670] [<c007afcc>] (SyS_finit_module) from [<c000e7e0>] (ret_fast_syscall+0x0/0x30)
    [   10.528184]  r6:00000000 r5:00000000 r4:00000000
    [   10.533006] Code: e34b3f0c ebff5f2d ea000030 e51b3020 (e5933000)
    [   10.539357] ---[ end trace 848ef228a453e3a5 ]---