This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于DM6446设备开启DSP dma问题



硬件环境:dm6446

软件环境:dvsdk2.0.0.22

问题描述:

        在dsp算法中,我想使用dma来进行算法优化,但是好像是在分配dma资源的时候出错了。

算法中关于dma部分的配置如下:

在server/*.cfg中:

DMAN3.heapInternal    = "L1DHEAP";       /* L1DHEAP is an internal segment */
// DMAN3.heapInternal = "DDRALGHEAP";    /* DDRALGHEAP is an external segment */
DMAN3.heapExternal    = "DDRALGHEAP";
DMAN3.idma3Internal   = false;
DMAN3.scratchAllocFxn = "DSKT2_allocScratch";
DMAN3.scratchFreeFxn  = "DSKT2_freeScratch";

DMAN3.paRamBaseIndex     = 80;  // 1st EDMA3 PaRAM set available for DMAN3
DMAN3.numQdmaChannels    = 8;   // number of device's QDMA channels to use
DMAN3.qdmaChannels       = [0,1,2,3,4,5,6,7]; // choice of QDMA channels to use
DMAN3.numPaRamEntries    = 48;  // number of PaRAM sets exclusively used by DMAN
DMAN3.numPaRamGroup[0]   = 48;  // number of PaRAM sets for scratch group 0
DMAN3.numTccGroup[0]     = 32;  // number of TCCs assigned to scratch group 0
DMAN3.tccAllocationMaskL = 0;   // bit mask indicating which TCCs 0..31 to use
DMAN3.tccAllocationMaskH = 0xffffffff; // assign all TCCs 32..63 for DMAN

在算法中也参照demo实现了IDMA3_Fxns接口函数,编译通过,运行时出现的错误截图如下:

对应的log信息如下: