AM3352的ADC作为普通ADC用时采样率能否配置为8K?在资料中没看到说明
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
可以的,看datasheet中描述
12-Bit Successive Approximation Register (SAR) ADC
• 200K Samples per Second
• Input can be Selected from any of the Eight Analog Inputs Multiplexed Through an 8:1 Analog Switch
• Can be Configured to Operate as a 4-Wire, 5-Wire, or 8-Wire Resistive Touch Screen Controller (TSC) Interface