TM4C1299KCZAD: TM4C1299KCZADI3R使用问题?

Part Number: TM4C1299KCZAD

我司使用TM4C1299KCZADI3R研发一款网口转串口产品K7-M4(内置PHY),在使用过程中出现以下问题,请协助分析可能的原因?
1.    K7-M4 与TP-LINK的8口交换机直连,当K7连接到交换机某一个网口时,网口灯不亮,通信失败,重新插拔网线,重启,更换网线均不能正常通信,此时,接交换机其他网口可以正常通信。(不能通信的端口是随机的)。
如下图,K7接交换机5口,可以正常通信,接交换机4口不能正常通信
2.    基于上述问题,我们更换K7-M4设备,重新测试,新设备接4口能够正常通信,但是接6口又不能正常通信。
3.    基于上述问题,客户还反馈一款交换机也有类似问题,交换机型号GY1010GE(利奇马)
4.    我们用有此问题的设备与笔记本电脑连接测试,笔记本,设备均使用静态IP,笔记本与此设备设置同一网段,也出现上述问题,有的笔记本可以与K7正常通信,有的不能建立连接,网口灯不亮。
5.    此产品我司出货量极大,客户反馈,每周均会发现2-3个有问题的设备,请协助分析可能的原因?需要改什么参数?