求大神解答:
在DM3730平台下我将1024个int型数据从DDR(SDRC)搬运到MCBSP2的FIFO中时,会出现硬中断丢失的情况,当搬移的数据越大时丢中断越明显,但是搬移1022个的时候又不会出现丢中断的情况(硬中断为timer6产生的64k中断)。
经测试发现如果数据从IRAM搬运到MCBSP2的FIFO就不会出现丢中断的现象。
感觉像是和总线有关,求大神解答一下。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Sun Jun,
请问单独只运行音频,是否就没有问题了?
你是否有使用EDMA,如是,你是否有调整音频EDMA所在的TC?