This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

c6678 镜像文件工具 疑问



请问各位技术支持及大神,hex6x.exe bconvert64x.exe b2i2c.exe b2ccs.exe romparse.exe ccs2bin.exe等工具怎么用?有相关文档吗?我看了bootloader.pdf也没看到说明,只是说用哪个哪个工具转换。

  • 核心是hex工具,可以参考C:\ti\ccsv5\tools\compiler\c6000_7.4.4\doc或类似目录下spru186文档hex工具章节。

    其余的工具都是用来做数据格式的转换,可以参考首页SPI boot的实例。

    另外bootloader文档的说明

    Utilities used to generate different table formats are listed below:
    • Hex6x is used to convert the application code into a boot table format.
    • Romparse is used to append the boot parameter to a boot table or a boot
    configuration table.
    • Bootconvert6x is used to convert the boot table derived from a little endian
    application code to a big endian format. This is required as the RBL assumes all
    the images to be in big endian mode.
    • B2i2c is used to convert the boot table into a i2c/spi format table. This table can
    be loaded into an EEPROM that is connected through I 2 C to the device.
    • Bootpacket is used to break the boot table into packets that can be sent from the
    host to the device booted in Ethernet boot mode.
    • Pcsendpkt is used to help the host send the packets generated by bootpacket to
    the boot device.