您好。
我看datasheet中对DDR2的PCB设计要求比较高,我是一个初学者,感觉设计DDR2的难度比较大,所以想在CMD文件中将所有的段都放在SHRAM中,有些问题:
1、如果我的代码不大,那么只用片内RAM,不外接DDR2和SDRAM,程序能否正常运行?
2、编写完代码怎么确定在运行时需要多大的RAM空间?
3、我最后生成的AIS文件的大小是33KB,那需要的RAM空间会大于33KB吗?
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.