This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAPL137-HT: DSP端代码格式选择eabi(ELF)和legacy COFF格式遇到的问题

Part Number: OMAPL137-HT

CCS版本12.8,C6000CGT版本8.3.12,输出文件格式为eabi(ELF),进调试模式后,代码全部正常,中断,主函数中的while循环点灯,都没问题;然后通过SPI_FLASH_WRITE.out烧写板载SPI FLASH,CCS中提示烧写完毕,校验也通过,板子断电然后上电,启动失败。然后改为7.4.8的CGT,仍然采用eabi(ELF),同样调试没有问题,烧入SPI FLAHS启动失败;将7.4.8的CGT输出格式改为COFF格式,进调试模式,仅while循环中的点灯代码运行正常,所有中断均无响应;将COFF格式的out文件烧入SPI FLASH,板子重启后点灯程序能运行,中断无响应。上述情况,我该怎么处理呢