AM3352: 升级uboot 从sdk 的2017 到2026,启动同一个fitimage 新的uboot 2026 出现Starting kernel ... 问题

Part Number: AM3352

我现在是将板子的uboot 从sdk 的2017 版本,升级到2026 版本,原本旧的uboot 是可以正常启动fitimage 的,且bootargs 配置为 'earlycon=ns16550a,mmio32,0x44e09000 console=ttyO0,115200n8 loglevel=8 root=/dev/ram0 rw', 可以正常看到kernel 启动log, 并正常启动,现在换成uboot 2026 版本后,bootargs 没变,还是 'earlycon=ns16550a,mmio32,0x44e09000 console=ttyO0,115200n8 loglevel=8 root=/dev/ram0 rw', 

=> bootm 0x88000000
## Loading kernel (any) from FIT Image at 88000000 ...
   Using 'conf-1' configuration
   Verifying Hash Integrity ... OK
   Trying 'kernel-1' kernel subimage
     Description:  Linux Kernel
     Created:      2011-04-05  23:00:00 UTC
     Type:         Kernel Image
     Compression:  uncompressed
     Data Start:   0x880113f0
     Data Size:    5902848 Bytes = 5.6 MiB
     Architecture: ARM
     OS:           Linux
     Load Address: 0x80300000
     Entry Point:  0x80300000
     Hash algo:    sha256
     Hash value:   dbc1b7373ca439fe70850915362be5991d21580c810c08f430ae67eaa0a65bea
   Verifying Hash Integrity ... sha256+ OK
## Loading ramdisk (any) from FIT Image at 88000000 ...
   Using 'conf-1' configuration
   Verifying Hash Integrity ... OK
   Trying 'ramdisk-1' ramdisk subimage
     Description:  Ramdisk Image
     Created:      2011-04-05  23:00:00 UTC
     Type:         RAMDisk Image
     Compression:  uncompressed
     Data Start:   0x885b26e8
     Data Size:    2108265 Bytes = 2 MiB
     Architecture: ARM
     OS:           Linux
     Load Address: 0x83000000
     Entry Point:  0x83000000
     Hash algo:    sha256
     Hash value:   f2adcb28abc8db029d08a70b44922d17181ef12d965b85a1aaa959d4058625e6
   Verifying Hash Integrity ... sha256+ OK
   Loading ramdisk from 0x885b26e8 to 0x83000000
## Loading fdt (any) from FIT Image at 88000000 ...
   Using 'conf-1' configuration
   Verifying Hash Integrity ... OK
   Trying 'fdt-1' fdt subimage
     Description:  Flattened Device Tree blob
     Created:      2011-04-05  23:00:00 UTC
     Type:         Flat Device Tree
     Compression:  uncompressed
     Data Start:   0x880000d0
     Data Size:    70204 Bytes = 68.6 KiB
     Architecture: ARM
     Load Address: 0x80200000
     Hash algo:    sha256
     Hash value:   922e664890d89e3e29510ceebcf806157170f2ac0492084f377b4ae4c9d527ac
   Verifying Hash Integrity ... sha256+ OK
   Loading fdt from 0x880000d0 to 0x80200000
   Booting using the fdt blob at 0x80200000
Working FDT set to 80200000
   Loading Kernel Image to 80300000
   Using Device Tree in place at 80200000, end 8021423b
Working FDT set to 80200000

Starting kernel ...

CCCCCCCC

上面出现Starting kernel ... 后大概等了30s 后出现CCCC, 板子重启,由于kernel 在旧的uboot 可以正常启动,且bootargs 起了作用,我现在怀疑是新的uboot 导致, 为什么新的uboot 下bootargs 没起作用,内核也没看到输出,不知道什么原因,大家有遇到过吗,能帮忙一下!

  • 板子的env 如下:

    => printenv
    arch=arm
    baudrate=115200
    board=am335x
    board_name=A33515BB
    board_rev=1.0
    board_serial=unknown
    bootargs=earlycon=ns16550a,mmio32,0x44e09000 console=ttyO0,115200n8 loglevel=8 root=/dev/ram0 rw
    bootcmd=run bootcmd_nand
    bootcmd_nand=echo Booting from primary nand image ...; mw.b 0x83000000 0xff 0x1000000; nand read 0x83000000 0x300000 0x1000000;bootm 0x83000000; echo Booting from backup nand image ...; mw.b 0x83000000 0xff 0x1000000; nand read 0x83000000 0x1300000 0x1000000;bootm 0x83000000
    bootcount=18
    bootdelay=2
    cpu=armv7
    eth1addr=04:23:22:68:0e:fa
    eth2addr=04:23:22:68:0e:f8
    ethaddr=04:23:22:68:0e:f8
    fdtcontroladdr=8df19510
    ice_mii=mii
    ipaddr=192.168.0.1
    loadaddr=0x82000000
    mtdids=nand0=nand.0
    mtdparts=mtdparts=nand.0:512k(spl),1m(u-boot),1m(u-boot.backup),512k(env),16m(fit),16m(fit.backup),80m(rootfs),80m(rootfs.backup),4m(config),4m(config.backup),53m(storage)
    netmask=255.255.255.0
    serial#=04:23:22:68:0e:f8
    serverip=192.168.0.10
    soc=am33xx
    stderr=serial@0
    stdin=serial@0
    stdout=serial@0
    vendor=ti
    ver=U-Boot 2026.01-ti-g5fb294342321 (Jul 09 2026 - 22:23:09 +0000)

    Environment size: 1079/131068 bytes

  • 您好

    已经收到了您的案例,调查需要些时间,感谢您的耐心等待

  • 你好,

    收到启动内核消息后,电路板似乎正在复位,ROM 引导加载程序进入 UART 引导模式,发送“CCCCC”。

    这是定制硬件还是EVM?

    您使用的是与最新 U-boot 对应的 Linux 内核,还是尝试使用旧内核?

    30 秒的延迟可能表明触发了 WDT 复位。因此,请在新的 Uboot 控制台上运行以下命令,检查是否有 WDT 信息,并分享输出日志。

    wdt list
    wdt dev

    问候,
    维努