This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

设备停在了starting kernel,不再继续



最近在移植am335x的板子,内核为sdk内的4.1.18,uboot是2014.7。

uboot启动没有问题,但是在最后starting kernel的时候卡住了。

在网上找到了一些方案比方说修改disable掉RTC(3.12.xx),在commandline里面选择ttyO0(使用的板子是在这个串口上),但是还是没有输出。

我的dtb文件出错会导致这一类的问题吗?还是说是我的内核编译的时候出现的问题。

以下是我编译的步骤:

./scripts/kconfig/merge_config.sh -m arch/arm/configs/omap2plus_defconfig ti_config_fragments/ipc.cfg ti_config_fragments/power.cfg ti_config_fragments/audio_display.cfg ti_config_fragments/system_test.cfg ti_config_fragments/baseport.cfg ti_config_fragments/wlan.cfg ti_config_fragments/connectivity.cfg ti_config_fragments/auto.cfg

make menuconfig ARCH=arm CROSS_COMPILE=arm-linux-gnueabihf-
在这一步,disable掉了RTC。

make -j4 uImage ARCH=arm CROSS_COMPILE=arm-linux-gnueabihf- LOADADDR=0x80008000

生成没有问题,但是无法启动。

以下是我的uEnv.txt

bootargs=console=ttyO0,115200n8 root=/dev/mmcblk0p2 rw rootfstype=ext4 mem=512M coherent_pool=8M rootwait loglevel=20
bootcmd=fatls mmc 0; fatload mmc 0 0x82000000 uImage;fatload mmc 0 0x80F80000 am335x-evm.dtb;bootm 0x82000000 - 0x80F80000
uenvcmd=fatls mmc 0; fatload mmc 0 0x82000000 uImage;fatload mmc 0 0x80F80000 am335x-evm.dtb;bootm 0x82000000 - 0x80F80000

这是我uboot启动时打印的:

U-Boot 2014.07 (Jun 03 2016 - 15:16:17)

I2C:   ready
DRAM:  512 MiB
NAND:  0 MiB
MMC:   OMAP SD/MMC: 0, OMAP SD/MMC: 1
*** Warning - readenv() failed, using default environment

Net:   <ethaddr> not set. Validating first E-fuse MAC
cpsw, usb_ether
Hit any key to stop autoboot:  0
WARNING: Could not determine device tree to use
switch to partitions #0, OK
mmc0 is current device
SD/MMC found on device 0
reading uEnv.txt
364 bytes read in 4 ms (88.9 KiB/s)
Loaded environment from uEnv.txt
Importing environment from mmc ...
Running uenvcmd ...
    97937   mlo
   441764   u-boot.img
  3500680   uimage
      364   uenv.txt
    39995   am335x-evm.dtb
     1559   readme.txt

6 file(s), 0 dir(s)

reading uImage
3500680 bytes read in 202 ms (16.5 MiB/s)
reading am335x-evm.dtb
39995 bytes read in 10 ms (3.8 MiB/s)
## Booting kernel from Legacy Image at 82000000 ...
   Image Name:   Linux-4.1.18Barney-gbbe8cfc
   Created:      2016-06-07  16:55:16 UTC
   Image Type:   ARM Linux Kernel Image (uncompressed)
   Data Size:    3500616 Bytes = 3.3 MiB
   Load Address: 80008000
   Entry Point:  80008000
   Verifying Checksum ... OK
## Flattened Device Tree blob at 80f80000
   Booting using the fdt blob at 0x80f80000
   Loading Kernel Image ... OK
   Loading Device Tree to 8fff3000, end 8ffffc3a ... OK

Starting kernel ...