This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Mcbsp0 Mcbsp1的冲突问题



各位TI工程师:

        配置Mcbsp1 EDMA3的接收,触发中断后用Mcbsp0的EDMA3发送,发现有冲突,Mcbsp0和Mcbsp1的EDMA3配置均是用CSL库进行配置的,在工作中发现有冲突,只有一个有作用!会不会是配置覆盖呢,假如我既要实现Mcbsp1 EDMA3接收,同时又要实现Mcbsp0 EDMA3发送,该如何实现?

  • 建议追踪一下EDMA寄存器配置,看看有没有重复配置

  • xinlu zhao 说:
    配置Mcbsp1 EDMA3的接收,触发中断后用Mcbsp0的EDMA3发送,发现有冲突,Mcbsp0和Mcbsp1的EDMA3配置均是用CSL库进行配置的,在工作中发现有冲突,只有一个有作用!

    你说的冲突现象是什么?是哪颗芯片?

    xinlu zhao 说:
    会不会是配置覆盖呢,假如我既要实现Mcbsp1 EDMA3接收,同时又要实现Mcbsp0 EDMA3发送,该如何实现?

    EDMA资源无非是通道channel映射,parameter set,如果怀疑冲突,则检查这两个资源是否用的同一个。