老师您好,我现在在用DM368 EVM的板子做视频编码,板子上有分量输入的接口,并且dvsdk的demo里面有选择分量输入的选项,但是我分量输入的时候demo运行报错:Error: Failed to create capture device. Is video input connected? 请问老师是什么原因,是需要配置什么东西吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Zhao Xin,
请问你的输入是720p么?
http://processors.wiki.ti.com/index.php/GSG:_Running_the_DVEVM_Demos#Starting_the_Standalone_Demo_on_DM365
With the DM365 EVM boards when you connect the EVM hardware, a pre-loaded example runs automatically on your video display. This example captures 720p component video and displays it as-is (i.e. without processing) to the connected HD display. The example runs automatically with no connection to a workstation in the default boot configuration. The DM365 EVM does not run the DVSDK demo out of flash out of the box.