66AK2L06可以用论坛提供的STK进行编译吗?我在更改了advance options -> Predefined Symbols ->Pre-define下 DEVICE_K2L与K2L_EVM,报编译出错,当将之前的DEVICE_K2H与K2H_EVM后报CSL_PCIeSerdesComEnable()函数未找到。软件环境安装了CCS6.1,MCSDK3_01_04_07,是否还要安装其他支持文件?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
66AK2L06可以用论坛提供的STK进行编译吗?我在更改了advance options -> Predefined Symbols ->Pre-define下 DEVICE_K2L与K2L_EVM,报编译出错,当将之前的DEVICE_K2H与K2H_EVM后报CSL_PCIeSerdesComEnable()函数未找到。软件环境安装了CCS6.1,MCSDK3_01_04_07,是否还要安装其他支持文件?
我也遇到了同样的问题,我用的是66AK2H12,也是所有要调用SERDES的测试例程都编译不过(SRIO、PCIE、GE、HyperLink),已经将Include和File Search修改至正确的路径,因为其他不调用SERDES的例程都可以编译通过(GPIO、I2C、Memory_Test、SPI、UART等),主要是报以下函数找不到:
CSL_***SerdesComEnable
CSL_***SerdesLaneConfig
CSL_***SerdesPllEnable
CSL_***SerdesShutdown
*** 表示:Ethernet / Hyperlink / PCIe / Srio
不知道上面的朋友找到解决方法没有??