This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

eMMC无法识别的问题

Other Parts Discussed in Thread: TPS65217

我的系统 在SD卡上执行的很好,但是复制到emmc后 执行到Waiting for root device /dev/mmcblk0p2...这个地方就停止了。我现在怀疑emmc移植的问题,

但是我不知道哪里错了,高手能不能帮我分析下。

[ 2.827819] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
[ 2.835998] ThumbEE CPU extension supported.
[ 2.840637] mux: Failed to setup hwmod io irq -22
[ 2.847045] Power Management for AM33XX family
[ 2.852172] Trying to load am335x-pm-firmware.bin (60 secs timeout)
[ 2.859100] Copied the M3 firmware to UMEM
[ 2.863647] Cortex M3 Firmware Version = 0x181
[ 2.868743]
[ 2.868743] The clk freq is 50000000
[ 2.874481] period_ticks is 2500
[ 2.878051] period_ticks is 2500
[ 2.881561] Prescaler value is 1
[ 2.885131] Prescaler value is 1
[ 2.888641] duty ticks is 2000
[ 2.899261] clock: disabling unused clocks to save power
[ 2.907867] Detected MACID=c4:ed:ba:88:7c:3c
[ 2.914916] #start __rtc_read_time
[ 2.918518] #__rtc_read_time
[ 2.921569] ##pcf8563_rtc_read_time
[ 2.926269] tm is secs=46, mins=58, hours=8,mday=14, mon=5, year=116, wday=2
[ 2.933807] #rtc_read_time
[ 2.936737] rtc-pcf8563 2-0051: setting system clock to 2016-06-14 08:58:46 UTC (1465894726)
[ 2.946777] Waiting for root device /dev/mmcblk0p2...

  • 大于等于4G的emmc要接在MMC1上,不能接在MMC0上的。先确认这点有没有违背。

    如果OK的话,查一下,你的kernel中是否有正常配置了emmc在emmc1上,可以参考beagleboneblack的配置,因为BBB板子就是emmc启动的。你发的log中,有用信息不多。你之前烧录写入的时候是一切正常的吗?

  • 是的,我们的EMMC是接在了emmc1上,而且原来我用的是bbblack的内核下载到我的emmc上,硬件电路应该是没问题的,

    配置我也查了下,和bbblack的配置视一样的。

    附件是我们的硬件电路

    代码如下,与emmc的相关代码我就添加了如下

    /* Module pin mux for mmc1 */
    static struct pinmux_config mmc1_common_pin_mux[] = {
    {"gpmc_ad3.mmc1_dat3", OMAP_MUX_MODE1 | AM33XX_PIN_INPUT_PULLUP},
    {"gpmc_ad2.mmc1_dat2", OMAP_MUX_MODE1 | AM33XX_PIN_INPUT_PULLUP},
    {"gpmc_ad1.mmc1_dat1", OMAP_MUX_MODE1 | AM33XX_PIN_INPUT_PULLUP},
    {"gpmc_ad0.mmc1_dat0", OMAP_MUX_MODE1 | AM33XX_PIN_INPUT_PULLUP},
    {"gpmc_csn1.mmc1_clk", OMAP_MUX_MODE2 | AM33XX_PIN_INPUT_PULLUP},
    {"gpmc_csn2.mmc1_cmd", OMAP_MUX_MODE2 | AM33XX_PIN_INPUT_PULLUP},
    {NULL, 0},
    };

    static struct pinmux_config mmc1_dat4_7_pin_mux[] = {
    {"gpmc_ad7.mmc1_dat7", OMAP_MUX_MODE1 | AM33XX_PIN_INPUT_PULLUP},
    {"gpmc_ad6.mmc1_dat6", OMAP_MUX_MODE1 | AM33XX_PIN_INPUT_PULLUP},
    {"gpmc_ad5.mmc1_dat5", OMAP_MUX_MODE1 | AM33XX_PIN_INPUT_PULLUP},
    {"gpmc_ad4.mmc1_dat4", OMAP_MUX_MODE1 | AM33XX_PIN_INPUT_PULLUP},
    {NULL, 0},
    };

    static void mmc1_init(int evm_id, int profile)
    {
    setup_pin_mux(mmc1_common_pin_mux);
    setup_pin_mux(mmc1_dat4_7_pin_mux);

    am335x_mmc[1].mmc = 2;
    am335x_mmc[1].caps = MMC_CAP_4_BIT_DATA | MMC_CAP_8_BIT_DATA;
    am335x_mmc[1].nonremovable = true;
    am335x_mmc[1].gpio_cd = -EINVAL;
    am335x_mmc[1].gpio_wp = -EINVAL;
    am335x_mmc[1].ocr_mask = MMC_VDD_32_33 | MMC_VDD_33_34; /* 3V3 */

    /* mmc will be initialized when mmc0_init is called */
    return;
    }

    static struct evm_dev_cfg a807_am335x_dev_cfg[] = {
    {am335x_rtc_init, DEV_ON_BASEBOARD, PROFILE_ALL},
    {clkout2_enable, DEV_ON_BASEBOARD, PROFILE_ALL},
    {tps65217_init, DEV_ON_BASEBOARD, PROFILE_ALL},
    {mii1_init, DEV_ON_BASEBOARD, PROFILE_ALL},
    {i2c1_init, DEV_ON_BASEBOARD, PROFILE_ALL},
    {i2c2_init, DEV_ON_BASEBOARD, PROFILE_ALL},
    {usb0_init, DEV_ON_BASEBOARD, PROFILE_ALL},
    {usb1_init, DEV_ON_BASEBOARD, PROFILE_ALL},
    {mcasp0_init,DEV_ON_BASEBOARD, PROFILE_ALL},
    {mmc1_init, DEV_ON_BASEBOARD, PROFILE_ALL},
    {mmc0_init, DEV_ON_BASEBOARD, PROFILE_ALL},
    {uart2_init,DEV_ON_BASEBOARD, PROFILE_ALL},
    {sgx_init, DEV_ON_BASEBOARD, PROFILE_ALL},
    {NULL, 0, 0},
    };

  • mmc1的初始化要放到前面,并且与mmc0的初始化间隔开,如下:我这样就通过了。

    {mmc1_init, DEV_ON_BASEBOARD, PROFILE_ALL}, 

    {mcasp0_init,DEV_ON_BASEBOARD, PROFILE_ALL},

    {mmc0_init, DEV_ON_BASEBOARD, PROFILE_ALL}, 

  • mmc1_init的初始化放到前面,并且与mmc0的初始化隔开,如下


    {mmc1_init, DEV_ON_BASEBOARD, PROFILE_ALL}, 

    {mcasp0_init,DEV_ON_BASEBOARD, PROFILE_ALL},

    {mmc0_init, DEV_ON_BASEBOARD, PROFILE_ALL}, 


  • 你的问题解决了吗?

    你是不是把sd卡里的所有镜像都复制到了emmc中了,然后从emmc启动的。而这个时候sd里没有任何镜像文件,但是sd还是插在板子上的啊?

    如果是这样的话,那么/dev/mmcblk0p2默认就是sd卡的。你把sd卡拔掉,系统应该就可以正常从emmc启动啦

  • 那如果是设备树的话,应该怎么修改啊?下面是我遇到的问题,看到的话,帮我分析一下呗!

    http://www.deyisupport.com/question_answer/dsp_arm/sitara_arm/f/25/t/131904.aspx