This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

FFTC协处理器的7.5kHz频率偏移问题。



在FFTC协处理器中一个模块的功能是用来实现7.5kHz的频偏的。

1. 我看了一下这个模块是在数据输入之前。这么说上行PUSCH信道的发端做完IFFT是无法做7.5kHz频偏的?必须要通过DSP编程实现的?

2. 如果PUSCH的发端IFFT可以通过FFTC协处理器配置7.5kHz频偏的话,我这么配置正确么?

SHIFT_DIR =0;

SHIFT_FACTOR=0;

SHIFT_PHASE=0;

SHIFT_INDEX=0;//选择16384

SHIFT_EN=1;

  • 可以做,FFT及IFFT只是direction不一样,FFT时是negative,IFFT配成positive,其他的配置方式是一样的,参考如下帖子,对于2048点,factor=2

    http://www.deyisupport.com/question_answer/dsp_arm/c6000_multicore/f/53/t/15278.aspx