This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于tms320c6713b芯片手册问题?

Other Parts Discussed in Thread: TMS320C6713B

1)tms320c6713b芯片手册48页中有一段备注:

‡ IPD = Internal pulldown, IPU = Internal pullup. [To oppose the supply rail on these IPD/IPU signal pins, use external pullup or pulldown resistors no greater than 4.4 kΩ and 2.0 kΩ, respectively.]

请问To oppose the supply rail on these IPD/IPU signal pins具体什么意思?是防止电源干扰的意思吗?

2)‡ IPD = Internal pulldown, IPU = Internal pullup. [To oppose the supply rail on these IPD/IPU signal pins, use external pullup or pulldown resistors no greater than 4.4 kΩ and 2.0 kΩ, respectively.]

§ To ensure a proper logic level during reset when these pins are both routed out and 3−stated or not driven, it is recommended to include an external 10 kΩ pullup/pulldown resistor to sustain the IPU/IPD, respectively.

上面两段话中我理解意思是一个要求上下拉电阻应不大于4.4 kΩ和2.0 kΩ,另一段要求上下拉电阻应为10 kΩ,这两段话是否相互矛盾?

请各位专家帮忙解答下,非常感谢!