This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

c6678l 上ipc和edma3之间是否有干扰



我在evmc6678l上单独测试edma3lld,拷贝1920*360大小的数据(ddr3拷贝到ddr3)时间大概是0.8个毫秒左右,但是如果加入了ipc的messageQ应用之后,同样的拷贝过程,需要5.6毫秒,这和之间内存拷贝时间差不多了,这是什么原因呢?请各位专家帮忙分析分析

  • 这和之间内存拷贝时间差不多了 

    [TY]请问这个 拷贝时间差不多了 怎么理解。用message Q 的话,您是用哪种copy方式,源地址和目的地址是否和edma3重合呢?

  • 你好,我测了一下,内存间直接赋值,时间相差只有1毫秒。另外:源地址和目的地址是否和edma3重合呢?这是什么意思,能否详细解释一下,谢谢!

    这个copy就是将yuv420格式的uv转换成yuv420sp格式的uv

    简单的内存之间的赋值:

    static void convertData(XDAS_Int8* outData,XDAS_Int32 yuvW,XDAS_Int32 yuvH)
    {
    int n=0;
    XDAS_Int8 *dest,*pu,*pv;
    pu=outData+yuvW*yuvH*3/2;
    pv=pu+yuvW*yuvH/4;
    dest=outData+yuvW*yuvH;
    memcpy(pu,dest,yuvW*yuvH/2);
    for(n=0;n<yuvW*yuvH/2;n+=2)
    {
    *(dest+n)=*pu;
    *(dest+n+1)=*pv;
    pu+=1;
    pv+=1;
    }
    Cache_wbInv(dest,yuvW*yuvH/2, Cache_Type_ALL, TRUE);
    }

    edma3://edma3的代码间附件,和sample差不多

    static void convertData(XDAS_Int8* jpgData,XDM1_BufDesc * outputBufDesc,XDAS_Int32 w,XDAS_Int32 h)
    {
    PROF_CLOCK begin;
    XDAS_Int8* start=jpgData+w*h;
    int i,n=1;
    if(outputBufDesc->numBufs<3)
    {
    printf("converData desc buf is smaller than 3\n");
    return;
    }
    for(i=1;i<12;i++)
    {
    if(w*i*2<32767 && h%(4*i)==0)
    n=i;
    }
    printf("@@@@@@@@@@@ src:0x%08x,0x%08x\n",outputBufDesc->descs[1].buf,start);
    begin=PROF_clock();
    edma3_copy(hEdma,(unsigned char*)outputBufDesc->descs[1].buf,(unsigned char*)start,1,w*n,h/(4*n),1,w*n,2,w*n*2,EDMA3_DRV_SYNC_AB);
    printf("%d decode frame 1:%f\n",MultiProc_self(),((float)(PROF_clock() - begin) / PROF_CLOCKS_PER_SEC));
    edma3_copy(hEdma,(unsigned char*)outputBufDesc->descs[2].buf,(unsigned char*)start+1,1,w*n,h/(4*n),1,w*n,2,w*n*2,EDMA3_DRV_SYNC_AB);
    Cache_wbInv(start,w*h/2, Cache_Type_ALL, TRUE);
    }