This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请教一个CCS连接错误的问题



使用CCS3.3、TI XDS560 PCI仿真器连接OMAPL138,一直好好的,昨天更改了一版内核起不来了,之后JTAG连接就提示如下错误:

SC_ERR_PATH_MEASURE

The measured lengths of the JTAG IR and DR scan-paths are invalid.
This indicates that an error exists in the link-delay or scan-path.

网上没搜索到可用的信息,请问这个问题通常在什么情况下发生?怎么解决?不胜感激!

  • 一般遇到这个仿真器怎么都连不上的问题

    确定是PC这边不是板子的问题,先把JTAG CLOCK降低试试,如果不行可能需要重装 CCS or 仿真器驱动 or 操作系统了

  • 谢谢,JTAG默认使用10.368M,改成5.184或1还是不行。改成串口启动方式,JTAG也报同样错误,同时上电或复位后也不发BOOTME(以前是可以的),只是在各种波特率下吐出不可显示的二进制数据。应该不是PC端的问题,因为修改内核之前一直用着,其它板子也是可以连接的。

    其实我就是把内核中board-da850-evm.c中Nand Flash分区的filesystem大小从固定值修改为MTDPART_SIZ_FULL,烧写完成后重启,串口输出有读取内核的过程,但是没有了解压内核的过程,而且从此以后JTAG就这样报错了,看来这个板子是被我玩坏了啊!

  • 你可以用nand工具把nand全擦掉,JTAG应该能连上,一般修改软件不太可能把板子搞坏,除非不小心动到了某些硬件