This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6657 McBSP EDMA for I2S



您好, 这问题困扰我很久了

目前需要利用McBSP来控制I2S ADC

首先, 使用Loop-back模式来测试McBSP

若以McBSP Register来测试, 可以正确的完成测试。

 

但以实际使用, 是需要利用EDMA或Interrupt来完成

PDK所提供的范例是需要RTOS来执行

目前的计划是不打算使用TI的RTOS

先前有使用SPI的EDMA来控制SPI

故将SPI EDMA改写成McBSP EDMA

 

TX是给已知的数值, 利用loop-back模式

来测试RX是否正确

此执行结果只能执行一次正确的EDMA

其他重复执行EDMA控制, 结果均为0

 

完整程序如下:

 

 

请各位先进帮我看是哪里错误

或我忽略掉那个重点

若有相关资料也可以提供, 谢谢

 

 

撷取部分程序内容

main

void main (void)
{
    volatile Uint32 failFlag = FALSE;
    int i;
    int success = 0;

    // Initiate src/dst buffers
    Initiate_Buffers(TEST_ACNT, TEST_BCNT, TEST_CCNT, TEST_ACNT, TEST_ACNT, TEST_ACNT*TEST_BCNT,
                     TEST_ACNT*TEST_BCNT, (Uint32)srcBuf, (Uint32)dstBuf, CSL_EDMA3_SYNC_A);

    I2S_McBSP_Setup();
    I2S_Edma_Open((Uint32)srcBuf, (Uint32)dstBuf);

    // loop
    for (i=0; i<10; i++)
    {
        Initiate_Buffers(TEST_ACNT, TEST_BCNT, TEST_CCNT, TEST_ACNT, TEST_ACNT, TEST_ACNT*TEST_BCNT,
                         TEST_ACNT*TEST_BCNT, (Uint32)srcBuf, (Uint32)dstBuf, CSL_EDMA3_SYNC_A);
        I2S_Transfer((Uint32)srcBuf, (Uint32)dstBuf, BUF_SIZE);

        failFlag = Verify_Transfer(TEST_ACNT, TEST_BCNT, TEST_CCNT, TEST_ACNT, TEST_ACNT, TEST_ACNT*TEST_BCNT,
                                   TEST_ACNT*TEST_BCNT, (Uint32)srcBuf, (Uint32)dstBuf, CSL_EDMA3_SYNC_A);
        if (failFlag == TRUE)
            success++;
    }
    //Close EDMA channels/module
    I2S_Edma_Close();

    //Verify src/dst buffers after transfer

    printf("success = %d\n", success);
    printf("end of test\n");

}

I2S_McBSP_Setup

void I2S_McBSP_Setup (void)
{
    int i;
    CSL_McbspRegs *mcbspRegs = (CSL_McbspRegs *)CSL_Mcbsp0_CFG_DATA_REGS;

    // 1. Place the McBSP in reset by clearing the XRST, RRST, FRST, and GRST bits to 0 in SPCR.
    mcbspRegs->SRGR = 0;

    // 2 Set the CLKXM, CLKRM, FSXM, FSRM, CLKXP, and CLKRP bits to 1 in the pin control register (PCR).
    mcbspRegs->PCR = (CSL_MCBSP_PCR_FSXM_INTERNAL<<CSL_MCBSP_PCR_FSXM_SHIFT) |
                     (CSL_MCBSP_PCR_FSRM_INTERNAL<<CSL_MCBSP_PCR_FSRM_SHIFT) |
                     (CSL_MCBSP_PCR_CLKXM_OUTPUT<<CSL_MCBSP_PCR_CLKXM_SHIFT) |
                     (CSL_MCBSP_PCR_CLKRM_OUTPUT<<CSL_MCBSP_PCR_CLKRM_SHIFT) |
                     (CSL_MCBSP_PCR_CLKXP_FALLING<<CSL_MCBSP_PCR_CLKXP_SHIFT)|
                     (CSL_MCBSP_PCR_CLKRP_RISING<<CSL_MCBSP_PCR_CLKRP_SHIFT)|
                     0;

    mcbspRegs->SPCR =
#ifdef ENABLE_I2S_LOOPBACK
                   (CSL_MCBSP_SPCR_DLB_ENABLE<<CSL_MCBSP_SPCR_DLB_SHIFT) |
#endif
                     0;
    // 2. McBSP clocks and frames to internal clock source
    // 2a Set the CLKSM and FSGM bits to 1 in the sample rate generator register (SRGR).
    mcbspRegs->SRGR = (CSL_MCBSP_SRGR_GSYNC_FREE<<CSL_MCBSP_SRGR_GSYNC_SHIFT)|
                      (CSL_MCBSP_SRGR_FSGM_FSG<<CSL_MCBSP_SRGR_FSGM_SHIFT) |
                      (31<<CSL_MCBSP_SRGR_FPER_SHIFT) |
                      (15<<CSL_MCBSP_SRGR_FWID_SHIFT) |
#ifdef ENABLE_INTERNAL_CLOCK
                      // internal setting
                      (CSL_MCBSP_SRGR_CLKSM_INTERNAL<<CSL_MCBSP_SRGR_CLKSM_SHIFT) |
                      (16<<CSL_MCBSP_SRGR_CLKGDV_SHIFT) |
#else
                      // external setting
                      (7<<CSL_MCBSP_SRGR_CLKGDV_SHIFT) |
#endif
                      0;

    // 2b Set the CLKXM, CLKRM, FSXM, and FSRM bits to 1 in the pin control register (PCR).
    mcbspRegs->RCR = (CSL_MCBSP_RCR_RPHASE_DUAL_FRM<<CSL_MCBSP_RCR_RPHASE_SHIFT)|
                     (CSL_MCBSP_RCR_RWDLEN2_16BIT<<CSL_MCBSP_RCR_RWDLEN2_SHIFT) |
                     (CSL_MCBSP_RCR_RFIG_NO<<CSL_MCBSP_RCR_RFIG_SHIFT)|
                     (CSL_MCBSP_RCR_RDATDLY_1BIT<<CSL_MCBSP_RCR_RDATDLY_SHIFT) |
                     (CSL_MCBSP_RCR_RWDLEN1_16BIT<<CSL_MCBSP_RCR_RWDLEN1_SHIFT) |
                     0;

    mcbspRegs->XCR = (CSL_MCBSP_XCR_XPHASE_DUAL_FRM<<CSL_MCBSP_XCR_XPHASE_SHIFT)|
                     (CSL_MCBSP_XCR_XWDLEN2_16BIT<<CSL_MCBSP_XCR_XWDLEN2_SHIFT) |
                     (CSL_MCBSP_XCR_XFIG_NO<<CSL_MCBSP_XCR_XFIG_SHIFT)|
                     (CSL_MCBSP_XCR_XDATDLY_1BIT<<CSL_MCBSP_XCR_XDATDLY_SHIFT) |
                     (CSL_MCBSP_XCR_XWDLEN1_16BIT<<CSL_MCBSP_XCR_XWDLEN1_SHIFT) |
                     0;

    // 2c Clear the SCLKME bit to 0 in PCR.
    for (i = 0; i < 100; i++) {
        asm (" nop");
    }

    // 3 Bring the McBSP out of reset by setting the XRST, RRST, and GRST bits to 1 in SPCR.
    mcbspRegs->SPCR |= (CSL_MCBSP_SPCR_GRST_CLKG << CSL_MCBSP_SPCR_GRST_SHIFT) |
                       (CSL_MCBSP_SPCR_XRST_ENABLE << CSL_MCBSP_SPCR_XRST_SHIFT) |
                       (CSL_MCBSP_SPCR_RRST_ENABLE << CSL_MCBSP_SPCR_RRST_SHIFT);

    //11. start internal frame sync generator
    mcbspRegs->SPCR |= (CSL_MCBSP_SPCR_FRST_FSG << CSL_MCBSP_SPCR_FRST_SHIFT); //Enable FRST

    for (i = 0; i < 2; i++) {
        asm (" nop");
    }
    //10.
    if (!(mcbspRegs->SPCR & CSL_MCBSP_SPCR_XEMPTY_MASK))  // Feed DXR if XSR is empty.
        mcbspRegs->DXR = 0xaa55;

//    while((mcbspRegs->SPCR & (1<<18)));
//    while(!(mcbspRegs->SPCR & 0x00000100));

}

I2S_Edma_Open

void I2S_Edma_Open (Uint32 srcBuf, Uint32 dstBuf)
{
    // EDMA Module Initialization
    CSL_edma3Init(NULL);

    // EDMA Module Open
    hModule = CSL_edma3Open(&moduleObj, CSL_TPCC_2, NULL, &EdmaStat);

    // McBSP_0 transmit Channel Open - Channel 37 for Tx (MCBSP0_XEVT)
    chParam.regionNum  = CSL_EDMA3_REGION_GLOBAL;
    chSetup.que        = CSL_EDMA3_QUE_0;
    chParam.chaNum     = CSL_EDMA3_CHA_37;

    hChannel37 = CSL_edma3ChannelOpen(&ChObj0, CSL_TPCC_2, &chParam, &EdmaStat);
    chSetup.paramNum   = chParam.chaNum; //CSL_EDMA3_CHA_37;
    CSL_edma3HwChannelSetupParam(hChannel37, chSetup.paramNum);

    // McBSP_0 receive Channel Open - Channel 36 for Rx (MCBSP0_REVT)
    chParam.regionNum  = CSL_EDMA3_REGION_GLOBAL;
    chSetup.que        = CSL_EDMA3_QUE_0;
    chParam.chaNum     = CSL_EDMA3_CHA_36;

    hChannel36 = CSL_edma3ChannelOpen(&ChObj1, CSL_TPCC_2, &chParam, &EdmaStat);
    chSetup.paramNum = chParam.chaNum; //CSL_EDMA3_CHA_36;
    CSL_edma3HwChannelSetupParam(hChannel36, chSetup.paramNum);

}

I2S_Edma_Setup_Params

void I2S_Edma_Setup_Params (Uint32 srcBuf, Uint32 dstBuf, Uint32 Size)
{
    CSL_McbspRegs *mcbspRegs = (CSL_McbspRegs *)CSL_Mcbsp0_CFG_DATA_REGS;
    // Clear Event of DMA3CC (Evt36, Evt37)
    EDMA3CC_SECRH           = 0x00000030;
    // Parameter Handle Open
    // Open all the handles and keep them ready
    paramHandle0            = CSL_edma3GetParamHandle(hChannel37, CSL_EDMA3_CHA_37, &EdmaStat);
    paramHandle1            = CSL_edma3GetParamHandle(hChannel36, CSL_EDMA3_CHA_36, &EdmaStat);

    // transmitter
    paramSetup.aCntbCnt     = CSL_EDMA3_CNT_MAKE(TEST_ACNT, (TEST_BCNT));
    paramSetup.srcDstBidx   = CSL_EDMA3_BIDX_MAKE(TEST_ACNT, 0);
    paramSetup.srcDstCidx   = CSL_EDMA3_CIDX_MAKE(0, 0);
    paramSetup.cCnt         = TEST_CCNT;
    paramSetup.option       = CSL_EDMA3_OPT_MAKE(FALSE, FALSE, FALSE, TRUE, CSL_EDMA3_CHA_37,
                              CSL_EDMA3_TCC_NORMAL, CSL_EDMA3_FIFOWIDTH_NONE, FALSE,
                              CSL_EDMA3_SYNC_A, CSL_EDMA3_ADDRMODE_INCR, CSL_EDMA3_ADDRMODE_INCR);
    if( ((Uint32)srcBuf & 0xFFF00000) == 0x00800000)
        paramSetup.srcAddr  = (Uint32)(global_address((Uint32)srcBuf));
    else
        paramSetup.srcAddr  = (Uint32)(srcBuf);
    paramSetup.dstAddr      = (Uint32)&(mcbspRegs->DXR);
    paramSetup.linkBcntrld  = CSL_EDMA3_LINKBCNTRLD_MAKE(CSL_EDMA3_LINK_NULL, 0);
    CSL_edma3ParamSetup(paramHandle0, &paramSetup);

    // receiver
    paramSetup.aCntbCnt     = CSL_EDMA3_CNT_MAKE(TEST_ACNT, TEST_BCNT);
    paramSetup.srcDstBidx   = CSL_EDMA3_BIDX_MAKE(0, TEST_ACNT);
    paramSetup.srcDstCidx   = CSL_EDMA3_CIDX_MAKE(0, 0);
    paramSetup.cCnt         = TEST_CCNT;
    paramSetup.option       = CSL_EDMA3_OPT_MAKE(FALSE, FALSE, FALSE, TRUE, CSL_EDMA3_CHA_36,
                              CSL_EDMA3_TCC_NORMAL, CSL_EDMA3_FIFOWIDTH_NONE, FALSE,
                              CSL_EDMA3_SYNC_A, CSL_EDMA3_ADDRMODE_INCR, CSL_EDMA3_ADDRMODE_INCR);
    paramSetup.srcAddr      = (Uint32)&(mcbspRegs->DRR);
    if( ((Uint32)dstBuf & 0xFFF00000) == 0x00800000)
        paramSetup.dstAddr  = (Uint32)(global_address((Uint32)dstBuf));
    else
        paramSetup.dstAddr  = (Uint32)dstBuf;
    paramSetup.linkBcntrld  = CSL_EDMA3_LINKBCNTRLD_MAKE(CSL_EDMA3_LINK_NULL, 0);
    CSL_edma3ParamSetup(paramHandle1, &paramSetup);
}
  • 附件是mcbsp的例子,不是C6657上的,但是EDMA3和MCBSP模块是一样的,你可以参考对比一下。

  • Hi Allen:

    我使用的是mcbsp_edma的例子, 想请问

    1. 在范例中在mcbsp的设定, 都是使用CSL_mcbsp的function

    在C6657的PDK内没有这些function

    所以就直接设定McBSP参数, 同先前提问中的I2S_McBSP_Setup

    这样是否可行

    2. EDMA部分, 依原先C6454的设定,修改成C6657

    C6657的mcbps在event 36及event 37

    故修改了regionAccess.draeh = 0xffff

    #define CSL_EDMA3_CHA_REVT0  36

    #define CSL_EDMA3_CHA_XEVT0  37

    但结果都无法进入中断, 请帮忙看问题发生在什么地方, 谢谢.

    完整程序

     

    程序如下

    void mcbsp_edma_setup (
        void
    )
    {
        CSL_McbspRegs *mcbspRegs = (CSL_McbspRegs *)CSL_Mcbsp0_CFG_DATA_REGS;
        CSL_Edma3ParamHandle     hParamBasic;
        CSL_Edma3ParamHandle     hParamBasic1;
        CSL_Edma3ParamSetup      myParamSetup;
        CSL_Edma3ParamSetup      myParamSetup1;
        CSL_Edma3ChannelObj      ChObj, ChObj1;
        CSL_Edma3ChannelAttr     chParam;
        CSL_Edma3Context         edmaContext;
        CSL_Edma3Obj             edmaObj;
        CSL_Edma3QueryInfo       info;
        CSL_Edma3CmdIntr         regionIntr;
        CSL_Edma3CmdDrae         regionAccess;
        Uint32                   i, j;
        CSL_BitMask16            ctrlMask;
            
        for (i = 0, j = 1; i < DATATX_COUNT; i++, j++) {
            srcBuff[i] = j;
            dstBuff[i] = 0;
        }
    
        /* Intc Module Initialization */
        intcContext.eventhandlerRecord = EventHandler;
        intcContext.numEvtEntries = 10;
    
        CSL_intcInit(&intcContext);
    
        /* Enable NMIs */
        CSL_intcGlobalNmiEnable();
    
        /* Enable Global Interrupts */
        intStat = CSL_intcGlobalEnable(&state);
    
        /* Opening a handle for the Event edma */
        vectId = CSL_INTC_VECTID_4;
        hIntcEdma = CSL_intcOpen(&intcObjEdma, CSL_INTC0_CPU_3_2_EDMA3CCINT0,//CSL_INTC_EVENTID_EDMA3CC_INT0,
                                 &vectId, &status);
    
        /* Edma Module Initialization */
        CSL_edma3Init(&edmaContext);
    
        /* Edma Module Level Open */
        hModule = CSL_edma3Open(&edmaObj, CSL_TPCC_2/*CSL_EDMA3*/, NULL, &status);
    
        /* Query Module Info */
        CSL_edma3GetHwStatus(hModule,CSL_EDMA3_QUERY_INFO, &info);
    
        /********************************Setup for Tx******************************/
    
        /* Setup the DRAE Masks */
        regionAccess.region = CSL_EDMA3_REGION_GLOBAL;//CSL_EDMA3_REGION_0;
        regionAccess.drae   = 0;
        regionAccess.draeh  = 0xFFFF;
    
        CSL_edma3HwControl(hModule, CSL_EDMA3_CMD_DMAREGION_ENABLE, &regionAccess);
    
        /* Open transmit channel */
        chParam.regionNum = CSL_EDMA3_REGION_GLOBAL;//CSL_EDMA3_REGION_0;
        chParam.chaNum = CSL_EDMA3_CHA_XEVT0;
        hChannel37 = CSL_edma3ChannelOpen(&ChObj,
                            CSL_TPCC_2,//CSL_EDMA3,
                            &chParam,
                            &status);
    
        /* Channel setup */
        hParamBasic = CSL_edma3GetParamHandle(hChannel37, CSL_EDMA3_CHA_XEVT0, &status);
    
        /* param setup */
        myParamSetup.option = CSL_EDMA3_OPT_MAKE(CSL_EDMA3_ITCCH_DIS, \
                                                 CSL_EDMA3_TCCH_DIS, \
                                                 CSL_EDMA3_ITCINT_DIS, \
                                                 CSL_EDMA3_TCINT_EN, \
                                                 CSL_EDMA3_CHA_XEVT0, \
                                                 CSL_EDMA3_TCC_NORMAL, \
                                                 CSL_EDMA3_FIFOWIDTH_32BIT, \
                                                 CSL_EDMA3_STATIC_DIS, \
                                                 CSL_EDMA3_SYNC_A, \
                                                 CSL_EDMA3_ADDRMODE_INCR,\
                                                 CSL_EDMA3_ADDRMODE_INCR \
                                                );
        myParamSetup.srcAddr = (Uint32)srcBuff;
        myParamSetup.dstAddr = (Uint32)CSL_MCBSP_0_TX_EDMA_REGS;
        myParamSetup.aCntbCnt = CSL_EDMA3_CNT_MAKE(4, 16);
        myParamSetup.srcDstBidx = CSL_EDMA3_BIDX_MAKE(4, 0);
        myParamSetup.linkBcntrld = CSL_EDMA3_LINKBCNTRLD_MAKE(CSL_EDMA3_LINK_NULL, 1);
        myParamSetup.srcDstCidx = CSL_EDMA3_CIDX_MAKE(0, 0);
        myParamSetup.cCnt = 1;
    
        CSL_edma3HwChannelSetupParam(hChannel37, CSL_EDMA3_CHA_XEVT0);
        CSL_edma3HwChannelSetupQue(hChannel37, CSL_EDMA3_QUE_1);
    
        CSL_edma3ParamSetup(hParamBasic, &myParamSetup);
    
        CSL_edma3HwChannelControl(hChannel37, CSL_EDMA3_CMD_CHANNEL_DISABLE, NULL);
        CSL_edma3HwChannelControl(hChannel37, CSL_EDMA3_CMD_CHANNEL_CLEAR, NULL);
    
        /* clear the error registers */
        chErrClear.missed = TRUE;
        chErrClear.secEvt = TRUE;
        CSL_edma3HwChannelControl(hChannel37, CSL_EDMA3_CMD_CHANNEL_CLEARERR, &chErrClear);
        CSL_edma3HwChannelControl(hChannel37, CSL_EDMA3_CMD_CHANNEL_ENABLE, NULL);
    
        /********************************Setup for Rx******************************/
    
        /* Open Receive channel */
        chParam.regionNum = CSL_EDMA3_REGION_GLOBAL;//CSL_EDMA3_REGION_0;
        chParam.chaNum = CSL_EDMA3_CHA_REVT0;
        hChannel36 = CSL_edma3ChannelOpen(&ChObj1,
                            CSL_TPCC_2,//CSL_EDMA3,
                            &chParam,
                            &status);
    
        /* Channel Setup */
        hParamBasic1 = CSL_edma3GetParamHandle(hChannel36, CSL_EDMA3_CHA_REVT0, &status);
    
        /* Param Setup */
        myParamSetup1.option = CSL_EDMA3_OPT_MAKE(FALSE,FALSE,FALSE,TRUE,\
                                                  CSL_EDMA3_CHA_REVT0, \
                                                  CSL_EDMA3_TCC_NORMAL, \
                                                  CSL_EDMA3_FIFOWIDTH_32BIT, \
                                                  CSL_EDMA3_STATIC_DIS, \
                                                  CSL_EDMA3_SYNC_A, \
                                                  CSL_EDMA3_ADDRMODE_INCR, \
                                                  CSL_EDMA3_ADDRMODE_INCR \
                                                 );
        myParamSetup1.srcAddr = (Uint32)CSL_MCBSP_0_RX_EDMA_REGS;
        myParamSetup1.dstAddr = (Uint32)dstBuff;
        myParamSetup1.aCntbCnt = CSL_EDMA3_CNT_MAKE(4, 16);
        myParamSetup1.srcDstBidx = CSL_EDMA3_BIDX_MAKE(0, 4);
        myParamSetup1.linkBcntrld = CSL_EDMA3_LINKBCNTRLD_MAKE(CSL_EDMA3_LINK_NULL, 1);
        myParamSetup1.srcDstCidx = CSL_EDMA3_CIDX_MAKE(0, 0);
        myParamSetup1.cCnt = 1;
    
        CSL_edma3HwChannelSetupParam(hChannel36, CSL_EDMA3_CHA_REVT0);
        CSL_edma3HwChannelSetupQue(hChannel36, CSL_EDMA3_QUE_1);
        CSL_edma3ParamSetup(hParamBasic1, &myParamSetup1);
    
        EventRecord.handler = &eventEdmaHandler;
        EventRecord.arg = (void*)(hModule);
        CSL_intcPlugEventHandler(hIntcEdma, &EventRecord);
    
        /* Enabling event edma  */
        CSL_intcHwControl(hIntcEdma, CSL_INTC_CMD_EVTENABLE, NULL);
    
        /* Hook up the EDMA Event with an ISR */
        EdmaEventHook(CSL_EDMA3_CHA_XEVT0, txmyIsr);
        EdmaEventHook(CSL_EDMA3_CHA_REVT0, rxmyIsr);
    
        /* Enable the interrupts */
        regionIntr.region = CSL_EDMA3_REGION_GLOBAL;//CSL_EDMA3_REGION_0;
        //regionIntr.intr   = (1 << CSL_EDMA3_CHA_XEVT0) | (1 << CSL_EDMA3_CHA_REVT0);
        //regionIntr.intrh  = 0;
        regionIntr.intr   = 0;//(1 << CSL_EDMA3_CHA_XEVT0) | (1 << CSL_EDMA3_CHA_REVT0);
        regionIntr.intrh  = (1 << 4) | (1 << 5);
        CSL_edma3HwControl(hModule, CSL_EDMA3_CMD_INTR_ENABLE, &regionIntr);
    
        /* Disable cahnnels and clear the EDMA event registers */
        CSL_edma3HwChannelControl(hChannel36, CSL_EDMA3_CMD_CHANNEL_DISABLE, NULL);
        CSL_edma3HwChannelControl(hChannel36, CSL_EDMA3_CMD_CHANNEL_CLEAR, NULL);
    
        /* clear the error registers */
        chErrClear.missed = TRUE;
        chErrClear.secEvt = TRUE;
        CSL_edma3HwChannelControl(hChannel36, CSL_EDMA3_CMD_CHANNEL_CLEARERR, &chErrClear);
    
        /* Enable the receive channel */
        CSL_edma3HwChannelControl(hChannel36, CSL_EDMA3_CMD_CHANNEL_ENABLE, NULL);
    
        /* Enable MCBSP transmit and receive */
    #if 0
        ctrlMask = CSL_MCBSP_CTRL_TX_ENABLE | CSL_MCBSP_CTRL_RX_ENABLE;
        CSL_mcbspHwControl(hMcbsp, CSL_MCBSP_CMD_RESET_CONTROL, &ctrlMask);
    #endif
    //    if (!(mcbspRegs->SPCR & CSL_MCBSP_SPCR_XEMPTY_MASK))  // Feed DXR if XSR is empty.
    //        mcbspRegs->DXR = 0xaa55;
    
        WAIT_FOR_1_CLK;
    
        /* wait for Transmit complete Interrupt */
        while (!intFlag);
    
        /* wait for Transmit complete Interrupt */
        while (!rxintFlag);
    
        /* Disable cahnnels and clear the EDMA event registers */
        CSL_edma3HwChannelControl(hChannel36, CSL_EDMA3_CMD_CHANNEL_DISABLE, NULL);
        CSL_edma3HwChannelControl(hChannel37, CSL_EDMA3_CMD_CHANNEL_DISABLE, NULL);
        CSL_edma3HwChannelControl(hChannel36, CSL_EDMA3_CMD_CHANNEL_CLEAR, NULL);
        CSL_edma3HwChannelControl(hChannel37, CSL_EDMA3_CMD_CHANNEL_CLEAR, NULL);
    
        /* clear the error registers */
        chErrClear.missed = TRUE;
        chErrClear.secEvt = TRUE;
        CSL_edma3HwChannelControl(hChannel36, CSL_EDMA3_CMD_CHANNEL_CLEARERR, &chErrClear);
        CSL_edma3HwChannelControl(hChannel37, CSL_EDMA3_CMD_CHANNEL_CLEARERR, &chErrClear);
    
        CSL_edma3ChannelClose(hChannel36);
        CSL_edma3ChannelClose(hChannel37);
        CSL_edma3Close(hModule);
        CSL_intcClose(hIntcEdma);
    }
    
  • 请问你的问题解决了吗,最近一直在做这个,好久了都没搞定

  • 很抱歉这问题摆放了很久
    我最终没有找到解决方法, 项目只好停摆了.