This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

dm368 emac



您好:请问我想把DM368的uboot  EMAC设固定到100Mbps怎么设定?

我需要把PHY去掉接到基带,可以去掉也接上了基带但是带宽不是100M,

我看了DATESHEET

• 2.5 MHz at 10 Mbps

• 25 MHz at 100 Mbps

不知道怎么设定这个 ,请教下怎么设定带宽,谢谢!