请问ths8200 支持50帧和60帧BT1120输入吗?如果支持需要怎么配置8200
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Lynn,
你是否有阅读过下面的帖子?
http://www.deyisupport.com/question_answer/dsp_arm/davinci_digital_media_processors/f/39/t/52747.aspx
Lynn,
- EVM和配置实例
关于TVP7002/THS8200,2个片子其实正好形成了一对收发,所以EVM板子我们也做成了一对EVM资料和寄存器表,请直接在http://www.ti.com.cn/tool/cn/tvp7002evm 上下载。
目前这2个片子具体支持了YPbPr/VGA的哪些分辨率, 数字接口是YUV444/422, 还是RGB, 都可以在配置表中的excel文件里找到。http://www.ti.com/cn/lit/zip/slec029 这个文档包括一个excel表,完整地列出了所有已经支持的分辨率和需要配置的寄存器的值;另外的inc和cmd文件其实就列出了哪些寄存器是格式相关寄存器和分辨率帧率相关寄存器。如果客户需要excel之外的分辨率配置,可以参考这个做相应修改。
你好;
Support for All ATSC Video Formats (Including 1080P) and PC Graphics Formats (up to UXGA at 75 Hz)
Video Synchronization by Hsync or Vsync Dedicated Inputs or by Extraction of Embedded SAV and EAV Codes According to ITU-R.BT601(SDTV) or SMPTE 274M and SMPTE 296M(HDTV)
可以支持的,具体看手册:http://www.ti.com/lit/ds/symlink/ths8200.pdf
在RDK的开发包中,有ths8200的驱动程序,具体路径:
DVRRDK_04.01.00.02/dvr_rdk/mcfw/src_linux/devices/ths8200
可以看看,这个驱动资料写得挺全的。